Hello Ninghan,
Generally speaking you will need to re-establish contacts between the port and the board. The piece should fit on top of the pads somewhat intuitively. The schematic for the EVM can be found on the DLP4500-C350REF page . Be sure that all…
Hi HF,
I have a generated a bmp file using python shown below and have saved it into flash, Doing this i am able to see proper image displayed from EVM.
Could you elaborate on how you are feeding it to the the EVM an in which operating mode?
Regards…
Hello Corentin,
Comparing with another EVM will help in isolating the issue to laptop setting or EVM.
Meanwhile, Could you please check the video out configuration of laptop by going "display setting " and selecting "advanced display setting" for windows…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLP4500 , DLPC350 Hi, apologies in advance, I have very little exposure to dlp products, so some terms and concepts are new to me, and my questions might be naive.
My goal is to download patterns…
Part Number: DLPLCR4500EVM The software was working fine with the earlier firmware but I uploaded a completely different firmware. Now my PC is not able to connect to the control software. Its showing an error "Unable to enter programming mode" when I…
Part Number: DLPLCR4500EVM Hi Experts,
Our customer would like to know which mode should be used to project a single image (logo) that is on a second monitor?. if it should be the pattern sequence, how should they use the second screen (connected to the…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLPC350
I have the following issue with my DLP LightCrafter 4500 Evaluation Module:
- The firmware was updated (memory writes took place, whereby the first 128 KB = bootloader size were not written…
Hi Kei,
I see that you are using 4 splash images based on the .ini file settings;
DEFAULT.PATTERNCONFIG.NUM_SPLASH 0x3 ; DEFAULT.SPLASHLUT 0x0 0x1 0x2 0x3 ;
Could you please check what are the image load timings of the splash images you are using and calculate…
Part Number: DLPLCR4500EVM Hi,
One day, I could not connect my DLP LightCrafter 4500 to my PC through USB. So I tried to update the firmware by pinning it to J18 and putting it into Programming Mode. However, it failed and the control software did not…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: DLP4500 , , DLPC350 Customer is already using DLP LightCrafter 4500 EVM GUI software.
Is there any "download phase shift profilometry /grey code library" for use with DLPLCR4500EVM or DLP4500?…