Part Number: DLPR300 Hi Team, Seeking your assistance if the application is possible.
So we are not using the DLP in a projector. We are trying to take multiple images out of DLP to use it into an application in quantum optics called four wave mixing…
Part Number: DLPR300 Other Parts Discussed in Thread: DLP4500 Hello,
We purchased a DLP® LightCrafter™ Evaluation Module ( www.ti.com/.../dlplightcrafter) as a projector for our clinic, but we face an issue when we use it to project our generated…
Other Parts Discussed in Thread: DLPC300 Dear All,
I'd like to ask you the writing option of the endian(big or little) for the DLPR300PROM writing to the FLASH by the ROM writer tool. We are building our DLPC300 original board without DM365.
Which…
Hello Marin and welcome to the E2E forums!
Before delving into further troubleshooting procedures, can you confirm that you have the most up-to-date software on your LightCrafter? Old software had RNDIS issues. The software can be found at www.ti.com/…
Ah, I understand now. Sorry for the confusion. To download the latest DLPC300 firmware, use this link: http://www.ti.com/tool/DLPR300
The rest of the system component firmwares are the in the previous link, which you attached a screenshot of.
-Paul …
Other Parts Discussed in Thread: DLPC300 , DLPR300 Which JTAG interface/device will be suitable for loading configuration data to the flash? What do I need, software utility side, to do this? This is on our own design not the lightcrafter evm - our mechanical…
Hi Chunde,
The .bin file for the DLPC300 is actually installed at C:\Program Files (x86)\Texas Instruments-DLP\DLP LightCrafter DLPR300 PROM, that is the default directory, in case you have not changed the directory location during the installation. …
Other Parts Discussed in Thread: DLPC300 , DLPR300 Hi,
I was attempting to update the DLPC300 and I put in a wrong file into the File box.(lcr_dm365_v5_nand.dat). The program stopped responding and now the light crafter doesn't even display the splash…
Hi,
Could you verify that you are on the latest versions of the FW for the DM365, MSP430, FPGA and DLPC300? I have listed the current versions as of today.
DM365: 5.0
MSP430: 3.0
FPGA: 2.6.43
^ These FWs are bundled here: www.ti.com/.../dlplightcr…
Hi Nick,
A few questions:
Did you update the DLPC300 FW with the EDID binary? If so, this would be a major issue. The DLPC300 FW is not included in the LightCrafter 3.0 SW bundle. You can find it here: http://www.ti.com/tool/dlpr300
Can you confirm you…