Art,
Yes, but you will need to download the correct firmware from the DLPR900 subdirectory that matches your DMD EVM in the GUI. You may have to use the boot hold jumper for the initial load.
Fizix
Hello Joselito,
E2E was down for maintenance until mid day yesterday. I am sorry for the inconvenience. Thank you for the response letting us know the versions you are using.
Apparently the bootloader on the "old" system is running since it has a heartbeat…
Part Number: DLPLCR67EVM Other Parts Discussed in Thread: DLPC900 , DLPLCRC900EVM , DLPLCR65EVM , DLPLCRC900DEVM , DLPR900 , DLPLCR50XEVM , DLPLCR90EVM , , DLP670S
Texas Instruments (TI) recently released new DLPR900 firmware (v 6.0) files for updated DLPC900…
Dear Fizix,
Sorry, I am quite new to the topic. If I order DLP6500FLQ, will I receive controller DLPR900 or DLPLRC900DEVM automatically or do I have to do extra order for DLP6500FLQ and for the controller?
Thank you, Jiri
Hello Leon,
Firmware v2.0.0 is NOT compatible with GUI 5.0.0. You will need to update the FW or revert to a much earlier version of the GUI.
GUI 5.0.0 requires FW 6.0.x which is available on ti.com. DLPR900 Firmware
Fizix
Hello again Winben,
Before you send this unit back, could you please try reloading the default OOB firmware that is in the DLPR900 folder for the 6500. If you do not have it, it can be downloaded from ti.com here:
https://www.ti.com/tool/DLPR900
Fizi…
Hello Shiqi Zhou,
Your board seems to be recognizing the controller well, the LEDs status shows that. What do you mean by 'buzzer'?
In Shivakumar's description, were you able to perform these tests?
1. You can verify the Flex cable between…
Hi Zhonghui,
Looking at the GUI status, It is clear that Controller is not able to communicate with DMD.
Please check if Flex Cable between controller and DMD board is proper and connected tightly. Make sure DMD is sitting on its holder properly. You can…
Hi Danilo,
Looking at the GUI Status, "Controller/DMD Incompatible" error bit is set. Which means Controller is not able to communicate with DMD.
In many cases, following below steps fixed the issue. 1. Make sure Flex cable and DLP6500FYE DMD…