Hi,
Mari Tsunoda said: What mode should they use? Basic or Enhanced? They want to know what HW connections they need to make. This is for EtherCAT usage.
The DP83826-EVM-AM2 PHY has ENHANCED mode is selected. So you can go with EnhancedMode.
…
Part Number: AWR2544LOPEVM Other Parts Discussed in Thread: AWR2544 , SYSCONFIG , , DP83TG720EVM-MC Tool/software: Hi,
I need help to enable DP83TC812 for AWR2544.
Currently I got a new task for the AWR2544, switch the auto phy from 1000Base-T1 DP83TG720…
Part Number: DP83826E Other Parts Discussed in Thread: , DP83826-EVM-AM2 Tool/software:
Hello.
I have some questions regarding the DP83826E.
Looking at the circuit of the DP83826-EVM-AM2, I see that the LED are driven by a MOSFET, whereas in another…
Part Number: MCU-PLUS-SDK-AM261X Other Parts Discussed in Thread: DP83826-EVM-AM2 , SYSCONFIG Tool/software: Hi Experts,
I am using AM261x-LP with MCU_PLUS_SDK for AM261x v10.00.01.10. For CPSW Based networking examples, I am unable to configure MII…
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: AWR2544 , Tool/software: Hi Expert, We are using DP83TG720S-Q1, on both our board and TI AWR2544 EVM board, the crystal not work, no signal. The power supply are OK, and reset is high.
Can…
Hello,
Yes, two DP83TG720 PHYs can be connected back-to-back as proposed. It is best to have some controller for configuration to easy any debug if the need arises similar to the EVM.
Regards,
Undrea
Hi Jim,
What are you evaluating the DP83TG720 for? If you can help me understand the application or specific standard you want to pass, I can help you.
If you just want to use the DP83TG720MC-EVM for network communication, you can just hook up the…
Hi Jim,
DP83TG720 is PHY_ID = 08 on this EVM. To read register 0x871, type "0871" in the Register Address field.
To read register 0x1 on the DP83867, please select PHY_ID = 00, and type " 0001" in the Register Address field.
Thanks,
David