Part Number: DRV10970 Hi Team.
Would you share your mailing list for sending email because
I'd like to ask quesions with my confidential information?
Thanks
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 HI
WE have a costumer that needs a driver for a small BLDC motor. WE have acquired your DRV10970 EVM board with DRV10970 drver that fits the specification. The settings used on EVM boards…
Part Number: DRV10970 Other Parts Discussed in Thread: DRV8306 Good Morning,
I'd like to ask some clarifications about the concept of the Hall placement (when using trapezoidal mode) concerning the DRV10970 component. I understand the difference between…
Part Number: DRV10970 Good Morning,
I have a question concerning the current limit function of the DRV10970 part number.
Inside the datasheet it is stated that the maximum output peak current is 1.5A; also, the current limit threshold can be set by connecting…
Part Number: DRV10970 Hi,
my customer wants to use DRV10970 but the Lock detect time of tlock_en of 0.7s is too long when motor braking and commutation. How can we shorten lock detect time?
Thanks,
Rui
Part Number: DRV10970 Hello.
I am trying to use the Maxon EC motor with TI drv 10970 single chip motor driver.
But it is not easy to use drv 10970.
I have to control speed and position of the motor.
I am using 12V 3 phases 3 hall sensor motor. ex. maxon…
Part Number: DRV10970 Other Parts Discussed in Thread: DRV10987 , DRV10974 , MCT8316Z , DRV8306 tHi Team,
we were evaluating the evaluation board of DRV10970 with our motor.
During experiment we found that the current waveform of motor phase is good a…
Part Number: DRV10970 Hi team,
My customer is surveying discrete motor stall detection solution. We saw TI document which mentioned hall sensor to implement stall detection feature to protect motor structure. If you have any advice, please let me know…
Part Number: DRV10970 Other Parts Discussed in Thread: DRV8306 , Hello Team,
I want hall sensored based BLDC driver IC which has integrate MOSFET and which can support current up 2A to 3A and voltage upto 24V.
so the output from this IC would be direct…