Part Number: DRV10970 Hi:
I want to ask about the DRV10970, now ,I drive the motor at 30 rotations per second, but the torque is very small, and it stops with slight load. Sometimes the 5s can be restored, and sometimes it stops completely. I need…
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 Hi all Would you mind if we ask DRV10970EVM? There is the description "Add three external pulls resistors for hall input across three jumpers J5, J7, and J8" on the EVM's document.…
Part Number: DRV10970 My custmor want to use DRV10970 to controll three-phasebrushlessDC motors,The attachment is the parameter of the motor.
Please help to confirm whether it is in line with the application.
Part Number: DRV10970 Other Parts Discussed in Thread: DRV8306 Team,
One of my customers has a mechanism in their system that they’d like to remain locked using the BLDC motor – they were hoping to keep the DRV10970 in Brake Mode (Shorting all Phases…
Part Number: DRV10970 Other Parts Discussed in Thread: DRV8308 , DRV8307 , I am in the process of selecting a motor driver/controller and I have narrowed it down to the DRV10970, DRV8308 or DRV8307. I need to drive Faulhaber 2-pole BLDC motors from 1000…
Part Number: DRV10970 Other Parts Discussed in Thread: DRV10974 , DRV10866 Hi team,
My customer use the 25kHz PWM to control the speed of motor.
In the previous post, you have mentioned that the resolution of the PWM is about 0.2% for DRV10970.
So I want…
Part Number: DRV10970 Hi,
Is there a case that the motor rotates in reverse if setting to low or high by using the motor direction control pin FR and changing the phase from 120° to 180° ?
Best regards, Kato
Part Number: DRV10970 Hi team,
According to the diagram of the DRV10970, My customer want to know below information:
1. The MOSFET is connect to the VM, what's the cap value between the Drain and Source electrode?
2. Is there any requirement for…