Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 , DRV8306EVM Hello,
I have an DRV109070EVM Evaluation Module here to drive an DF45M024053-A2 Brushless Motor from Nanotec.
The motors main datas are: rated valtage: 24V, rated current: 2…
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 Hi all Would you mind if we ask DRV10970EVM? There is the description "Add three external pulls resistors for hall input across three jumpers J5, J7, and J8" on the EVM's document.…
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 , DRV10983 , DRV10987 Can the DRV10970 Evaluation Module drive a 3-phase brushless DC motor with no Hall sensors?
The motor, for a tangential blower, has only 3 wires.
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 Hello,
I've searched through the forum but couldn't find a solid answer, so I'm hoping my post is not a duplicate.
I have an application where I currently have a brushed DC…
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 , I got my evaluation board and provided 12V power supply. However VINT is only about 0.19V. During my power ON and OFF through S1 switch, I did see the VINT =4.97 V at one point but that…
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 Hello,
I'm confused about how to connect the Hall sensors to the DRV10970EVM from my 3 phase brushless motor. The motor has 5 wires for the Hall sensors - Vcc, GND, and one to each of…
Part Number: DRV10970EVM Other Parts Discussed in Thread: DRV10970 , DRV10975 , DRV10974 I am running the DRV10970 with a Maxon 339267 BLDC, with an input voltage of 12V. I am able to spin the motor without issue in trapezoidal mode, however in the desired…
Hi Enes,
TIDUBH6 refers to the TIDA-00919 where we have the Hall ICs but the connectors are not part of this. These connectors are part of DRV10970EVM.
If the Hall is a digital sensor, we connect HP of all three phases to the IC and HN is pulled to VINT…
Part Number: BOOSTXL-DRV8320RS Other Parts Discussed in Thread: LAUNCHXL-F280049C , DRV10970EVM , C2000WARE I'm using BOOSTXL-DRV8320RS on a LAUNCHXL-F280049C to drive our 6V BLDC motor. Using the InstaSpin-FOC GUI, I Enable System and wait for the…