Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 I am using the drive plate of DRV10983Q1 to debug the motor. The motor control requirement is to switch the speed of the motor from 100 to 400, and the switching interval is 1.5 seconds…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: USB2ANY , DRV10983 , DRV10987 Hello,
I too am having an issue I can't get around regarding a write error:
DRV10983 USB2ANY.lvclass:Write
Register.vi<ERR>
Register writing not successful…
Part Number: DRV10983Q1EVM hello i am sung myung working for amotech co.
I am turning the drive ic.
and i recognize that the difference rpm is occurred with same pwm duty signal on the motor.
When i ratate motor with 20% pwm duty first. motor's rpm is…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 Hi there, I purchased the DRV10983Q1 EVM and after looking at the display tab of the GUI, the values seem to be incorrect (for example its displaying the supply voltage as 0V even…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 Hi there,
I have been trying to drive a bldc motor with the drv10983Q1 chip for the past couple days with no success. I have been successfully able to communicate with the device over…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983-Q1 , , USB2ANY , DRV10983 I'm trying to setup the motor parameters for a BLDC pump.
The phase to center tap resistance is measured at 0.5875 Ohms (half of the phase-to-phase resistance…
Part Number: DRV10983Q1EVM Other Parts Discussed in Thread: DRV10983 , USB2ANY I tried all the suggestions in the thread previously on this, with no luck. I still get the following message: "
Register.vi<ERR> Register reading not successful!!…
Hey Nathan,
Since the part is returned, about to go through failure analysis, and we've been having some back and forth with Viktorija. I will close this thread and continue offline.
Best,
-Cole
Dear Brian,
Thanks for your suggestion. Now by new USB2ANY working good with DRV10983Q1EVM.
Now i am programmed with manual parameter and driven the motor it start's & stop's. Again with some time delay start & stops. My response graph show below(Before…
Part Number: DRV10983Q1EVM Hi TI support team.
As I asked before, I'm using DRV10983Q1.
I had some problem but figured out thanks to your advice.
Now I have another issue about the DRV10983Q1
Recently, I changed two things.
First I selected regulator…