Part Number: DRV11873 Other Parts Discussed in Thread: DRV10982-Q1 , DRV10983-Q1 , MCT8316Z-Q1 Hi team
Could you help give an automotive device with similar spec to DRV11873? My customer chosen DRV11873 on a prototype board and now the customer needs a automotive…
Part Number: DRV11873 Other Parts Discussed in Thread: DRV10983 , Dear Sir/Ms.
We have customers who use DRV10983 to design fans, and the terminal has defective products. It was found that PIN12 (5V) and PIN16 (PWMIN) were burned. The customer asked the…
Part Number: DRV11873 Other Parts Discussed in Thread: DRV10974 Hello,
My customer has been using LB11685AV(ON Semi), but it will be EOLed, so they have to find an alternative motor driver soon. If I checked cross reference, it gave me DRV11873. However…
Part Number: DRV11873 Hi team,
Here's an issue from the customer may need your help:
The motor speed cannot be increased to around 5000. With a 5V 150mA supply, increasing the supply voltage or increasing the duty cycle, the motor will stop spinning…
Part Number: DRV11873 Hi team,
Issue: Is it okay to pull up the RD to 3.3 V? Or it can only connect to V5 or VCC (12V) ? The specification states that the pin is open-drain, although it is pulled up to V5 or VCC. So is the open drain output 3.3V OK?
Could…
Part Number: DRV11873 Other Parts Discussed in Thread: DRV10970 , Hi Team,
For 3W small motor in 300 rotating speed, could we reach 0.01% accuracy, which means 0.03?
Do you any recommendation?
Part Number: DRV11873DRV11873 has no output in my application.
I made the following confirmation and attempt
1.Test the impendence to GND of U/V/W of DRV11873
OK PCBA: about 5MΩ (with the Motor connectted to drv11873)
NG PCBA:about 200Ω …