Part Number: DRV134 Other Parts Discussed in Thread: DRV135 , INA137 , INA134 , INA1651 I would like to have a single differential transmitter (DRV134 / DRV135) drive up to 50 differential receivers (INA134 / INA137). The idea is to have a line level audio…
Part Number: DRV134 Other Parts Discussed in Thread: TINA-TI Hi all, Drv 134 is giving gain more than 6 dB .It is nearly 6.7 dB what may be the reasons for my problem?
Part Number: DRV134 Hi,
As per datasheet, the operating temperature range for DRV134UA/1K is -40degC to +85degC.
We are looking for -55degC to +125degC part in the same package. As per datasheet, -55degC part is only available for PDIP/SOIC 8 pin device…
Part Number: PCM1821EVM Other Parts Discussed in Thread: PCM1821 , PCM4201 , DRV134 Hi
PCM1821 transmits 32-bit two-channel data. The customer's product actually only has a mono signal. When the back-end MCU receives the I2S dual-channel data, it needs to…
Part Number: DRV134 Other Parts Discussed in Thread: INA134 , PGA2311 Hello,
I'm designing a preamp around the PGA2311 and I'm using the DRV134 and INA134 chips to facilitate balanced I/O. I want to maintain the largest signal swing I can within…
Part Number: DRV134 Other Parts Discussed in Thread: OPA1632 Hello!
I have a improvent suggestion for the DRV134:
the input for that IC should be selectable non symetrical and symetrical.
So this device can be used for a non symetrical and symetrical…
Hi Mehmet,
Our line driver portfolio features single-ended to differential like DRV134 and DRV135 or differential to single-ended like DRV6xx family. Perhaps you can just look into fully-differential op amps: Fully differential amplifiers | TI.com
Best…
Part Number: DRV134 Other Parts Discussed in Thread: INA217 , TINA-TI Hai,
I am using DRV134 device as line driver in my audio bus application. The bus consists of two DRV134 devices with the outputs shorted together i.e +V0 of one device is shorted with…