Part Number: DRV2604L Hello,
we are using a DRV2604L with the LRA C08-00A.003 (Precision Microdrives).
Supply Voltage of the system is at approx. 2.8V
LRA Parameters: Rated voltage: 1.2V, Frequency: 240Hz
Unfortunately, we are not able to run an autocalibration…
Part Number: DRV2604 What would be the recommended way to immediately stop a DRV2604 waveform executing from RAM, or to at least verify that no waveform is currently running, in order to update the program data? I've tried clearing the GO bit, but this…
Part Number: DRV2604-2605_DESIGN_TOOL Hi:
I'm using DRV2604 to drive an ERM vibrator. Please provide me the detailed explanation of each field in Design Tool.
Thanks
Part Number: DRV2604 Hi team,
My customer would like the alternative for IIS2DHTR (STMicro).
Could you please tell me any recommend?
They will use it as fall detection for human.
Thanks.
Part Number: DRV2604 [urgent]Please let me know the position of the first pin in the actual sample. We attached the figure. Please mark around the first pin.
Part Number: DRV2604 Hi,
When selecting our haptics drivers products, it is important to compare which features are supported by the devices and which of them are required for the end application. Here there are some useful questions that may help for…
Part Number: DRV2604 Other Parts Discussed in Thread: , DRV2624 Hello,
What are the key differences between the DRV2604, DRV2604L and the DRV2624L?
At the moment we are considering the DRV2604L for our application, because it is availble in a VSSOP package…
Part Number: DRV2604
regarding this post, does the answer in the forum post applies to both the auto-calibration and diagnostic modes?
https://e2e.ti.com/support/motor-drivers/f/38/p/546736/1995117?tisearch=e2e-quicksearch&keymatch=DIAG_RESULT#19951…
Part Number: DRV2624 Other Parts Discussed in Thread: DRV2604 Hi DRV driver gurus,
I am trying to understand the major differences between DRV2624 and DRV2604. My current design uses 2604 but I am considering migrating to 2624, if it makes sense.
Are…