Part Number: DRV2700 Hi Team,
Referring to the DRV2700EVM, we designed a 3-way piezoelectric ceramic driver circuit. However, I found that after DRV2700 is enabled to work, it will interfere with some other digital signals on the board, causing significant…
Part Number: DRV2700 Hi ,
Can you help me with design review for DRV2700 ?
in my design,
the input signal(sig_in) is 0 to 4.096V DC coupeld.
expected to output signal of 0 to 100V
output current is below 4 mA.
attached electrical scheme.
The most important…
Part Number: DRV2700 Other Parts Discussed in Thread: TPS8802 , Dear Team,
Do we have suitable solution can replace microchip RE46C100D8, thanks!
Condition
PWM input 3.3V or 5V
VDD 12-16VDC
add 3pin (Buzzer)
Many Thanks,
Jimmy
Part Number: DRV2700 Hi,
I am working on PZT driving circuits. I have come across the IC DRV2700. The output mentioned is the datasheet is is pulses. I would like to know whether the same IC can be used for ramp signal or sinusoidal signal for driving…
Part Number: DRV2700 Hello. ive been trying to understand how ca i use de inputs for this device. I guess that a can put a analog input at +IN pin and put the -In pin to gnd or a 0.1uf capacitor. Its is possible?
Part Number: DRV2700 Hi Team,
I use DRV2700 flyback mode as a high-volge power supply in my board. I refered DRV2700EVM-HV500 to design my circuit but cut the Pulldown Network and Integrator circuit.
Now I test output voltage is only 30V in net "HVPP",…
Part Number: DRV2700 Hello, My customer is looking for a piezo driver to meet the following requirements. Does DRV2700 can output 0 to 150V, not +/-100V? Vin = 0V to 10V Vout = 0 to 150V Iout = 20mA (max) Best regards, K.Hirano
Hi,
To clarify, are you seeing the boost drop issue with the default actuator? Your original post led me to believe you were using an external actuator. If you could monitor the current and voltage across the load on a scope and share those results that…