Hello,
Please answer following question from customer.
Q1:
Datasheet describe following.
Please let me known which VO1/2 waveform is correct when VS is 4.75V to 6V and expected VO1/2 waveform is 0.5V to 4.5V.
Q2:
VO1/2 output voltage range is restricted…
Hello,
Customer has a device it shows EEPROM CRC Check fail bit is “1”.
Please answer following question from customer.
Q1:
Please let me known the detailed method of EEPROM CRC check.
Q2:
Please advise if EEPROM data can be read out from…
Other Parts Discussed in Thread: DRV3201-Q1 Hi
My customer will use DRV3201-Q1. He has a question about Qg of FET for driving. Could you tell me about the following question?
There is the following sentence in datasheet. "Drives 6 Separate N-Channel Power…
Hello,
Please answer following question from customer.
ERR terminal goes high shortly when STAT0 is read by SPI in spite of VDS error is existing.
It can be understood because of error flag is cleared during short period of time .
Is Protective Action…
Hello,
Customer wants to know the SDO response for SPI invalid data input.
Please answer following questions.
Q1: When invalid write address is received at A, what data will send out from SDO at B?
Q2: When invalid write address is received at C, what…
Other Parts Discussed in Thread: DRV3201-Q1 Hello,
Please answer following question from customer.
They want to confirm if DRV3201-Q1 can be used for DC motor H-bridge pre-driver.
(Because they want to use same PC board for DC motor and 3 Phase Motor…
Other Parts Discussed in Thread: DRV3201-Q1DRV3201-Q1 About Programmable Dead Time function
Hi
My customer is using DRV3201-Q1. Could you let me know about the following?
- I understood that this function detects time between the high input voltage…
Hello,
Please advise if following fault detection works or not during Loss of clock detection test/VS comparator test.
1)VS undervoltage
2)VS overvoltage
3)Boost converter undervoltage
4)HS VDS error
5)LS VDS-error
6)Programmable dead time vi…
Other Parts Discussed in Thread: DRV3201-Q1 Hello,
Customer wants to know startup time of boost converter from B_EN changes to High.
I have already answer answered as follows.
“The time until the boost reaches it's final value is strongly depending on…