Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Hi,
I wanted to implement two Output capacitors at the output pin of DR5013-Q1 as shown in the Figure attached. I am implementing those due to checking of Conducted susceptibility at the…
Part Number: DRV5013-Q1 Hello guys,
One of my customers is considering using DRV5013-Q1 for their next products.
They have the following question about the device at the moment.
Could you give me your reply?
Q. We want to attach a capacitor between OUT…
Part Number: DRV5013-Q1 Hi,Staff
Please tell me how to calculate Vol (Output Loe Level voltage). I'm thinking of the following calculation, is there any problem?
Vcc=5V, Output-Pull up =1kΩ, Rds=50Ω
Vol = 5V/(1kΩ + 50Ω)×50Ω = 238mV(min…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Hello guys,
One of my customers is using DRV5013-Q1 for their BLDC motors.
They have an question about DRV5013-Q1 package structure as the follow.
Could you please give me your reply?
Q.…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Dear, Sir.
tON typical & maximum values are defined on the datasheet, page 6.
My customer is asking the duratuion of ON=Low after power-up.
Is it possible to clarify & assure about…
Part Number: DRV5013-Q1 Hello,
a customer would like ot know the maximum thermal load capacitance of P/N: DRV5013ADEDBZRQ1.
Can you please advise?
Thank you very much.
Best regards
Adnan
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Hello Team,
I got a question from customer about the DRV5013-Q1.
Q. Does DRV5013-q1 have internal clock? If yes, Do you know the frequency?
Customer want to know whether the clock frequency…
Part Number: DRV5013-Q1 Dear, Sir.
My customer is asking about the output when VCC is under 2.5V.
VCC range is defined from 2.7V to 38V.
According the datasheet description, I am gussing it would be Hi-Z?
Sorry to ask about this kind of matter. I would…
Part Number: DRV5013-Q1 Is there any DRV5xxx hall sensor working at 180 degree ambient operating temp? the application is for the servo motor.
It seems the E version can work up to 150degree only.
Regards
Brian