Part Number: DRV5013-Q1 Dear all,
I am designing a BLDC motor controller and because of the reduced size of the motor I have to use a magnetic enconder and employ 3 HALL sensors to determine rotor position.
I am reading some articles about how to choose…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5055 Dear Community
Use the Hall sensor to measure the angle of the DC motor. The measurement error is a requirement of ±1°. Do you have a Hall sensor that satisfies this?
Thanks.
Part Number: DRV5013-Q1 Hi Sir,
Per tidu835, pls give some advice about the distance between the magnet and sensor? or pls tell us the distance in this reference. The magnet used in this design, how much is the magnetic strength?
Part Number: DRV5013-Q1 Hi
What is the maximum value of Tr and Tf at pin "OUT" of DRV5013-Q1?
In the datasheet of the device, the tyipcal value is 200ns as Tr and 31ns as Tf. PLS let me know the maximum value at the same test condtions as shown in…
Part Number: DRV5013-Q1 Dear, Sir.
I would like to confirm following items. Please give your advice.
1)7.3.3 Power-On Time explains using Figure13, 14, 15.
tON looks start from the finish of VCC rising.
The other side, 7.1 Overview expaines this device…
Part Number: DRV5013-Q1 Dear, Sir.
My customer is considering to apply DRV5013-Q1 for their system, now.
On their system, There is a possibilty magnet would be stalled on magnetic field
BRP < B < BOP position and power up.
Figure 15 and description…
Part Number: DRV5013 Other Parts Discussed in Thread: SN74LVC3G17
Hi,
Q1. I would like advice on what to look out for when connecting DRV5013 to SN74LVC3G17. We need you to check the external components. <Conditions> ■ Operating temperature: 5~80°…
Other Parts Discussed in Thread: DRV5015-Q1 , DRV5013-Q1 , DRV5013 , DRV5011 Hello Team,
Please suggest latch type hall sensor which withstand lower temperature rating upto -55C. Package is not concern yet. Below are details of hall sensor specificatio…
Part Number: DRV5013-Q1
Hi All
In Fig. 13 and Fig. 14 of DataSheet, it becomes Low once at startup.
Please tell me the following about this behavior.
1, The time from H to L.
2, The time from L to H.
3, The time from H to the end of Ton.
Please also…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5013 Hi Champs,
I got question from my customer, can you please check attached xlsx file?
Best regards,
DRV5013_Question.xlsx