Part Number: DRV603 Other Parts Discussed in Thread: DRV602 , Tool/software: Hi,
I am considering replacing DRV602 with DRV603.
Q1. Is it possible to replace DRV602 with DRV603 with pin compatibility? Looking at the datasheet, it seems that the only…
Part Number: DRV602 Hi team,
My customer has a questions about DRV602, they want to know if there's any concern using it to drive 32 ohm and 320 ohm headphones since the data sheet suggests minimum load to be greater than 600 ohm.
Part Number: DRV602 Hi,
May I know the EN VIH minimum and maximum value?
In datasheet, only show the typical, my customer have meet enable voltage close to the VIH typ., some device can't normal enable.
They want to know the minimum and maximum…
Hi Luis, We can reproduce customer's problem with 5.2V VDD and 3.3V Enable signal on the DRV602 EVM. Here are my process: 1. Removed LDO and reset IC from the EVM. Sent 5V VDD and 3.3V EN externally. 2. Check DRV602 output by Audio Precision equipment…
Part Number: DRV602 Hi team,
my customer is looking for a headphone amp with headphone impedance detection (100 ~ 600 ohms). Do we have any line driver/headphone amp that can detect the headphone impedance, or any way to implement it with some external…
Part Number: DRV602 Hi,
My customer have meet DRV602 THD+N FAIL issue.
Schematic as below.
Do you have any suggestion for this issue.
Please add me friend or provide me your email address, I can provide more detail include full schematic, layout…
Part Number: DRV602 Other Parts Discussed in Thread: DRV603 Hi Sirs, The DRV603 and DRV602 are pin compatible devices while the DRV603 supports UVP function at pin 11 and can be left NC with the DRV602. Customer can have the options to assemble the DRV603…
Part Number: DRV602 Hi Sir,
I want to use DRV602 to replace MAX97220AETE, Would you please help review below circuit change to DRV602?
VDD=5V, is there have any relative resistor and capacitor need change?