Part Number: DRV8106-Q1 When DRVOFF is asserted on the DRV8106 which pull-down strength is used, the passive pulldown of about 150k Ohms or the Istrong pull down which draws a minimum of 30mA?
Part Number: DRV8143-Q1 Other Parts Discussed in Thread: DRV8874-Q1 , DRV8106-Q1 , DRV8706-Q1 Hello Team, customer wants to use the charge pump for additional reverse polarity circuit according our app note SLVA835A.
But we need the specification how much…
Sumeet,
The "H" version and "S" version are included in the same datasheet. Please see direct link below:
https://www.ti.com/lit/ds/symlink/drv8106-q1.pdf
Regards,
Ryan
Part Number: DRV8714-Q1 Other Parts Discussed in Thread: DRV8106-Q1 Hi team,
Can we use DRV8714-Q1's VCP to drive back-to-back FETs such that it can be used as reverse polarity protection as well as high side enable? Currently only reverse protection…
Hi
Thank you for your questions.
-Recommended to use under 150C for Tj in normal operation. TSD is kind of final guard/protection function under the fault/issue condition.
-Ioux=30A is for drive capability without thermal condition. Expecting short period…
Part Number: DRV8702D-Q1 Other Parts Discussed in Thread: DRV8106-Q1 , DRV8706-Q1 , DRV8705-Q1 Hi Expert,
Our customer has a new request. They are looking for 50A~70A motor driver solution. I see discrete H bridge gate driver + MOSFET may meet the requirement…
Part Number: DRV8703-Q1 Other Parts Discussed in Thread: DRV8106-Q1 , DRV8705-Q1 Hi,
customer want use DRV8703-q1 as high side driver. independent half bridge.
they want remove low side mos. that will report GDF error.
DRV8703-q1 GDF register all are only…
Hey Robert,
Basically the chip can handle 28V, but it isn't really recommended to design your system fully around 28V. Think of the absolute max as "beyond this the device could be damaged even with momentary voltage spikes", and the recommended operating…
Hi
Thank you for your DRV proposal.
-DRV8714(4 CH half bridge), DRV8706(2CH half bridge), DRV8106(1CH half bridge) is good one to propose. These are gate driver, so external FET should drive their current requirement.
-Another option is DRV8245-Q1. This…