Part Number: DRV8145H-Q1EVM Tool/software: Looking at the EVM schematic, it looks like it should be fine to swap out the DRV8145H for the DRV8145H so long as R22, R25-28 are populated - can you confirm if that is correct or I am missing anything else? …
Part Number: DRV8145H-Q1EVM
Tool/software:
According to the circuit timing requirements in the manual:
Apply 12V power to VM and VCP to trigger POR (Power-On Reset).
After NFAULT is pulled low for more than 3.5 ms:
A low pulse of 30 μs on SLEEP…
Part Number: DRV8145H-Q1EVM Tool/software: I run the GUI and connect the evaluation board to my laptop.
When teh board is plugged in, the GUI gives the message "Please wait while the device connection is in progress..." After this messages disappears…
Hey Rafael,
Please connect it to Ground. You can check out the EVM hardware files to see an example layout: https://www.ti.com/tool/DRV8145H-Q1EVM
Best,
Jacob
Part Number: DRV8245S-Q1LEVM Other Parts Discussed in Thread: DRV8706S-Q1EVM
Dera Team,
I am working on DRV8245S-Q1 EVM now I have to connect DC high torque motor in connect as HS mode and run, as show in attached pic but when its go about to 1.2A…