Part Number: DRV8213 Tool/software: Hello fellows,
I'm using the to implement a control mechanism to move come mechanism in both directions, with equal time spent in each direction.
To achieve this, I'm driving the mechanism with a triangular waveform…
Part Number: DRV8213 Tool/software: Hi Sir,
We want to find a solution to replace GMT G2015 (constant current type 1-ch H-bridge driver IC) and we suggest DRV8213. Customer think it's too complex. Do we have simple solution for controlling camera's…
Part Number: DRV8213 Hi Sir,
Please refer to the attached file, when the DRV8213 boot up, why the nFault pin has the pull down about 126us?
DRV8213RTER_nFault_issue.docx
The nFault pin has added a pull-up 10KOhm to VM_3.3V.
Part Number: DRV8213EVM While the EVMs for DRV8213-14-34 parts are OK, they would be much more useful if some of the many unused pins on the MSP430 were made accessible. This would allow them to be used for more flexible prototyping.
Even better, it would…
Part Number: DRV8213 Hello,
To understand the failure modes of the IPROPI pin of the DRV8213, I wanted to ask if either of the configurations occurring in an instantaneous event would damage with the IPROPI clamp and VREF value or overall performance…
Part Number: DRV8213 Hi Sir,
My customer would like to use the DRV8213 for the E-shutter driver application, could you please help to review the schematics and advise comments?
The reverse and forward current both are 250mA, switching timing is 25 msec…
Part Number: DRV8213 Hi team,
/FAULT and /STALL pin are open-drain output, but there is pull-up source inside of IC when I see the block diagram. If i use Vcc=3.3V, is there any issue by pull-ed up to 1.8V externally in order to connect to 1.8V MCU?
…
Part Number: DRV8213 Other Parts Discussed in Thread: DRV8832 , This new part looks interesting indeed, compared to the DRV8832 I used some time ago.
When will samples be available? DSG and/or RTE packages?
blessings, Tim
Part Number: DRV8215EVM Other Parts Discussed in Thread: DRV8212 , DRV8213 , DRV8215 , DRV8214 Tool/software: Hello,
I am interested in using one of your DRV821X series components. Mainly, I am interested in the Evaluation Boards of the DRV8212, DRV8213 …
Part Number: DRV8213EVM Other Parts Discussed in Thread: DRV8213 , DRV8214EVM , , DRV8214 Tool/software: Hi team,
Could you use the DRV8214EVM to evaluate the DRV8213 properly too?
Thank you.
Kind regards,
Wouter Kragt