Part Number: DRV8231A Dear all,
I know that presumably, there will be nothing such as a SPICE model for the DRV8231A. Still, I want to make sense of voltage/current waveforms I am measuring by scope when driving a small, conventional (brushed) DC Motor…
Part Number: DRV8231A Hello,
We are using the DRV8231A in a battery-operated application for driving solenoids. In our design, the sleep-mode quiescent current is critical and must remain below 1 µA, as specified in the datasheet.
However, we observed…
Part Number: DRV8243-Q1 Hi team,
Regarding the specifications on page 78 , we have identified two dimension issues in the recommended diagram.
As indicated by the red arrows in the image below, some dimensions are missing.
Could you please provide…
Part Number: DRV8231A I have two sets of boards (from two different asssembly houses). One set has a couple of boards (out of 10) exhibiting the EXACT restart problem described in Application Note SLVAG26. The other set of boards hasn't shown this problem…
Part Number: DRV8231A Other Parts Discussed in Thread: INA241A , DRV8876 , DRV8231 Tool/software: Hi Team,
My customer now wants to use DRV8231A as motor driver. And they have accuracy requirement as Iout < 0.05A; error < 5mA. and Iout< 0.15A error…
Part Number: DRV8231A Other Parts Discussed in Thread: DRV8231 Hi,
Our customer is considering driving a buzzer using an H-bridge to increase sound pressure. We selected the DRV8231A based on the following requirements. Is this acceptable? Buzzer voltage…
Part Number: DRV8231A Tool/software: Hi,
We are currently evaluating the DRV8231A for replacing a discrete circuit. However, during operation, I have encountered an issue where the IC fails under certain conditions. Below is a summary of the application…
Part Number: DRV8231A Tool/software: Hi team,
It seems that the current mirror error get large if R_IPROPI is small(100ohm to 500ohm ). Is there any recommendation value of R_IPROPI? Best regards, Goto