Part Number: DRV8231A Other Parts Discussed in Thread: DRV8231 , Driving a 12V geared motor (100:1 Metal Gearmotor 20Dx44L mm 12V CB) in a configuration to push paper.
We have used this configuration for over 40,000 cycles without an issue.
On the…
Part Number: DRV8231A Hi Team,
we using DRV8231A in our circuit
Motor voltage VM = 9 V Motor current trip point ITRIP 900 mA VREF voltage VREF = 3.3 V IPROPI resistance RIPROPI= 1.5 kΩ how to know Stall IPROPI voltage trip point VIPROPI,STALL Voltage…
Part Number: DRV8231A Hi team,
I found IIPROPI peak current is recommended 3mA in DRV8231A datasheet, So as AIPROPI is 1500uA/A, Does it mean DRV8231A only can sense 2A motor current? but datasheet says output current can be up to 3.7A.
Regards…
Part Number: DRV8231A Other Parts Discussed in Thread: DRV8231 , DRV8220 , DRV8242-Q1 , DRV8256 , DRV8876-Q1 , DRV8847 , DRV8908-Q1 , DRV8912-Q1 , DRV8847EVM Tool/software:
Hi,
We have been using the DRV8837CDSGR in the past, and due to our voltage…
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8874 , DRV8231A Tool/software: Hi team,
May I get the SOA curve of MOSFET for DRV8874 and DRV8231A?
BR
Amber
Part Number: DRV8231A Tool/software: I have a handful of drivers that internally shorted with and without catastrophic failure of the case.
- All pins with the exception of VM and VREF are shorted to ground.
- VREF is ~500 ohms to ground and VM…
Part Number: DRV8231A Hello,
My application drives several valves with a DRV8231A. IN1 and IN2 signals are controlled by a 0V or 3V signal from a microcontroller.
A valve needs 1.2A to open or to close. Power supply is 6V. VREF is set to 2.5V (Itrip…
Part Number: DRV8231A Other Parts Discussed in Thread: DRV8870 Hi team,
We want to replace DRV8870 with DRV8231A. We were testing DRV8231A and found that motor current controlled by DRV8231A was smaller than that controlled by DRV8870 when the motor…
Part Number: DRV8231A Other Parts Discussed in Thread: DRV8837 , Hello,
I saw this kind of question posted for DRV8837 here but wanted to check if the same would be true for DRV8231A.
Application: AC pile charging inlet lock
Issue:
Customer…