Part Number: DRV8244S-Q1LEVM Other Parts Discussed in Thread: UNIFLASH , MSP430G2553 Hello TI expect,
I try to connect DRV8244S-Q1EVM board by DRV824x_DRV814x-Q1EVM-GUI tool. Anyway, it's always stuck as below once I click connect icon.
I'm not…
Part Number: DRV8244S-Q1LEVM Hello,
I am using a DRV8244S-Q1LEVM motor driver which is apart of the VQFN-HR package. I am having some trouble with finding the operating current of a motor based on the ADC in value that is passed in to my MR-CANHUBK344…
Part Number: DRV8244S-Q1LEVM Hi TI team, the link to the cloud-based GUI is not working. Refer to the screenshot below. The DRV824 series tool seems to be missing.
I retrieved the old link, which is also not working (screenshot below) - Ankit
Part Number: DRV8244S-Q1LEVM Hello,
I've been trying to start up a DRV8244S by writing CLR_FLT to 1b. But it does not seem to wake the driver.
After examination, I found that device responds incorrect messages on SPI.
For example reading 0x00 register…
Part Number: DRV8244S-Q1LEVM Hi I need support in setting up the board. I have connected the board with Arduino pins
GND - GND
PIN 13 - SCLK
PIN 12 - SDO
PIN 11 - SDI
PIN 10 - nSCS
Register Map looks like this:
Can you share a sample Arduino…
Part Number: DRV8244S-Q1LEVM Hello,
Unfortunately 1 of our evaluation boards has damage, and I would like to make sure why exactly this happened. Our test setup was as following:
Board/Schematic: MD047A / Assembly 003
disconnected J4 PH/IN2_MCU…
Part Number: DRV8244S-Q1LEVM Other Parts Discussed in Thread: DRV8145-Q1 , DRV8706-Q1 , DRV8144-Q1 I am using the evaluation module for the DRV8244S motor driver to drive a load with the following test setup:
15V (max 40A) Power supply into J14 (Battery…