Part Number: DRV8245S-Q1LEVM [Test condition]
* PH/EN mode
* 20kHz/50% duty
Hi, I have DRV8245S-Q1LEVM(SPI, 'S' variant), and try to use SSC(Spread Spectrum Clocking) feature because of EMC.
On datasheet of DRV8245, i can enable/disable SSC function…
Part Number: DRV8245S-Q1LEVM Hi Team,
I have following request, can you please check and advise how we can support here?
"
We received the DRV8245S-Q1EVM, but no matter what I did for a week, the PC connection of the card could not be established…
Ahh yeah for that one check out DRV8145P-Q1LEVM , the "L" stands for leaded I recently learned. Or similarly for the Full-Bridge version /DRV8245S-Q1LEVM
Best,
Jacob
Hey Chae,
Typically 10kΩ is our default, though anything 1k to ~50k should work.
Chae Hui Cheon said: Is there an overall application circuit that I can refer to?
Best would be to download the EVM design files here: https://www.ti.com/tool/DRV8245S…
Part Number: DRV8145P-Q1LEVM Tool/software: Hello team,
Before we updated the firmware, the DRV8145P-Q1LEVM can be connected to GUI.
However, below message showed up and we performed the update.
After this update, GUI recognize this DRV8145P-Q1 LEVM…
Part Number: DRV8244-Q1 Other Parts Discussed in Thread: DRV8245S-Q1LEVM
The SPI (S) and SPI (P) versions of these chips are very similar - same specs, both SPI controlled. However, the key difference is that the (P) version uses an external 5V for the…
Hey Adam/Customer,
Adam Torma said: Current sense accuracy needs <15% with 1A to 2A.
Unfortunately I cannot guarantee any accuracy beyond what is shown in the datasheet, you'll need to test it in your system conditions and see if its accuracy will…
Hi,
Thank you for your feedback. I confirmed it link works.. Anyway could you try these one instead?
www.ti.com/.../DRV8245S-Q1LEVM
https://www.ti.com/lit/zip/slvc827
If both of them do not work, I guess you may have security wall or something..
reg…