Part Number: DRV8316C-Q1 Other Parts Discussed in Thread: DRV8316C , DRV8316 For my project i am looking fo a simple 3-PWM bldc motor controller, during my reacearce drv8316c did look like one of the best options.
The problem I have with this schematic…
Part Number: MCT8315Z Other Parts Discussed in Thread: DRV8316C , MCF8316C-Q1 , MCT8316AEVM , MCF8316A , MCF8316AEVM , MCT8316Z , DRV8316 , DRV8316REVM Hi There,
we are looking for a brushless DC motor controller/driver for our pump. We have two issues so far…
Part Number: DRV8316C-Q1 Other Parts Discussed in Thread: DRV8316 I am implementing C driver for the DRV8316C but I am facing issue with the SPI write.
By performing a read of all the registers, I get the following values :
IC Status : 0x00
Status register…
Hi Xiaofu,
Thank you for posting to the Motor Driver's forum!
The DRV8316-Q1 device, which is AEC-Q100 qualified for automotive applications, is a three-phase integrated FET device with a recommended operating voltage between 4.5V to 35V and a maximum…
Hi Tachibana-san,
For the UCC27710 device, will let someone from the power management group respond
I will follow up by end of this week with an updated response regarding DRV8316 device.
pinFMA might be a supporting document within DRV8316-Q1 PPAP but…
Hi Andrew,
This behavior is newly discovered so unfortunately I don't have all the answers to your questions yet. I am working with the team to fully understand this and to see if the datasheet needs to be updated or if there is a different solution.…
Hi Jerome,
Thanks for the information, I did some testing in lab and found the default register settings to be the same as what you saw, with the exception of register 07h which was 0. Correlating this with the datasheet for the DRV8316-Q1, it looks like…
Other Parts Discussed in Thread: DRV8316 , DRV8316REVM , MCT8316Z , MCT8316Z-Q1 , MCF8316A , MCT8316A , DRV8316-Q1 The DRV8316 and MCx8316 families of 3-phase integrated MOSFET BLDC motor drivers include an up to 200-mA adjustable buck regulator capable of outputting…
Part Number: DRV8316 Hi,
After initializing the DRV8316 registers, when I read the IC_Status register, the NPOR bit was set to 1.
Q1.Please tell me when the NPOR bit is set.
Q2. Is there any problem in operation even if the NPOR bit is set?
Q3.Is there…
Part Number: DRV8312 Other Parts Discussed in Thread: MCT8316Z , MCT8316A , MCF8316A , DRV8316 , DRV8329 , DRV8328 , DRV8300 , DRV8306 , MCT8316Z-Q1 We are required to drive a 3 phase 24V, 3.1A BLDC motor. It is a sensored motor with hall effect sensors built…