Part Number: DRV8312 Other Parts Discussed in Thread: MCT8316Z , MCT8316A , MCF8316A , DRV8316 , DRV8329 , DRV8328 , DRV8300 , DRV8306 , MCT8316Z-Q1 We are required to drive a 3 phase 24V, 3.1A BLDC motor. It is a sensored motor with hall effect sensors built…
Hello Zirui,
DRV8316-Q1 supports AEC-Q100, while DRV8316 does not (This is the meaning of "Q1" in the name). We would not recommend the 8316 or the 8316-Q1 because, as you said, this device cannot support the motor current of 5A (it has a maximum Irms…
Part Number: DRV3245Q-Q1 Other Parts Discussed in Thread: DRV8316 , DRV8316-Q1
Hi Team,
The customer is reviewing DRV3245Q-Q1 for the joystick steering project.
* Delete blocks.
If you have a better BLDC driver for the project, please recommend it.
Other Parts Discussed in Thread: MCT8316A , MCF8316A , DRV8311 , DRV8316 , DRV8353 , DRV8305 , DRV8323R , DRV8353R , DRV8323 , DRV10983 , DRV10983-Q1 , DRV10975 , DRV10987 I am seeking for a sensorless driver for the BLDC motor. Do you have any such product?? If yes…
Part Number: DRV8316
Hi Team,
The customer asked questions when connecting MCU to DRV8316.
It's a 5V MCU.
Question
Q1. The AVDD output voltage value is 3.3V, should the VREF be used as a 2.8V to 3.3V input?
Q2. Is the VREF value 5V value available…
Part Number: DRV8316 Hi,
The customer has a problem with the heat generation during DRV8316 operation.
The customer calculated thermal resistance value is 192 degrees.
TJ = P × R θ JC + TC [ ℃ ]
(0.6A * 12V) * 15.2 + 83 = 192
Q1 : Is the customer…
Part Number: DRV8316 Hello E2E,
May I ask you some questions ?
Q1.
I would like to use a DRV8312R in "Cycle-by-Cycle Current Limit mode".
In that case, can I leave the "SOA, SOB and SOC " pins open ?
Q2.
In 3x PWM mode,
A. All INLx…
Part Number: DRV8316 Hi Team,
Our customer is evaluating DRV8316REVM by SPI communication of external MCU (don’ t use TI MCU and GUI).
However, they can’t communicate to DRV8316REVM.
[Evaluation Status]
After reset, they read “Control__1…