Part Number: DRV8332-HT Other Parts Discussed in Thread: DRV8316C , DRV8316 , DRV8316REVM , DRV8876 , DRV8876EVM
Hello TI Team,
We are evaluating DRV8376H and DRV8316CT as potential replacements for DRV8332DKDR .
Could you please advise:
Which…
Part Number: DRV8332-HT Hello team,
iam uisng the DRV8332HDDV for the control of one three phase motor and the motor was operated on the 24v SUPPLY so the 24V is given as the input to the driver and based on the PWM the right phases are energized but…
Part Number: DRV8332-HT Tool/software: Hello.
I need to know the RDS(on) value of the DRV8332-HT however the Data sheets does not make it clear what it is.
In Features it says that RDS(on) is 80mΩ
In Electrical Characteristics is says that RDS(on…
Part Number: DRV8332-HT Other Parts Discussed in Thread: DRV8316C , DRV8376 Tool/software: Hello there,
Can you please let me know if you have any in stock for this item DRV8332DKDR or DRV8332DKD
Thank you,
Dhexter
Part Number: DRV8332-HT Tool/software: Hi Team,
Due to DRV8332DKDR EOL, BU suggest move to DRV8432DKDR.
Customer feedback DRV8432DKDR cannot direct replace DRV8332DKDR in their design-
1. Not P2P
2. Smaller current
3. Higher impedence
…
Part Number: DRV8332-HT Tool/software: We used the following circuit to drive the propeller, and there was a problem with one of the propellers during use: after the propeller was started, it ran normally. About half an hour later, the propeller had a…
Part Number: DRV8332-HT For DRV8332, if using six-step control, its power consumption will be smaller than using FOC control? Is this right? Since for six-step control, only two MOSFETS will be turned on during each step.
Part Number: DRV8332-HT Is the FAULT signal function still support or disable on DRV8332-HT? Is FAULT signal still detect for over current shut down or under voltage protection occurred? How long the FAULT signal stay LOW when error occurred?
Part Number: DRV8332-HT Hi support team,
I have read your explanations about disabled thermal shutdown in DRV8332-HT that date back to about 4 years ago, with the intention to make corrections to the confusing datasheet. Unfortunately, the datasheet…