Hi Jason,
Thanks a lot for your response. After doing the changes suggested by you, there is significant reduction in throttle response time.
Regards,
Premkumar T.
Part Number: DRV8353R I am using the DRV8353RS and have checked via SPI communication and only the GDUV error signal is active. The rest of the signals are consistent with the datasheet. However, I have a picture like the one in the datasheet and looking…
Part Number: DRV8353RS-EVM
Hi,
Please help for below queries.
1.
We don't want to use shunt resistor for motor phase sensing.
Instead of shunt resistors we are using hall sensor for motor phase sensing. - See Below reference image
Can we connect…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Dear Sir/ Madam,
I am looking for DRV8353RS spice model. It would be really helpful if you can please share.
Thanks and regards,
Poojitha.
Part Number: DRV8353RS-EVM
Hi,
I am using the DRV8353RS-EVM to operate the BLDC motor, and I am controlling the motor speed using the GUI. I pressed the RESET switch S2 (FSMJSMA), and the EVM board began signalling the fault. I then tried to connect…
Hi Joshua Maize,
As I mentioned above, I followed the above steps for the validation of the custom MOSFET board with DRV8353Rs board by isolating the DRV8353 MOSFETs and I removed the MOSFETs in the DRV8353 board.
When I supply the power to the DRV8353…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hello Team,
I am working on DRV8353 with F280015x interfacing with 48V ABZ+PWM Motor. On the UMC code I enabled the ABZ ENC feedback by enabling the "MOTOR1_ENC" macros for enabling the…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hello Team,
I am working on DRV8353 with F280015x interfacing with 48V PMSM Motor with Hall feedback . At no load conduction Motor is working fine, motor all 3-phase current are same.
A…
Hi Youngtak,
Similarly closing this thread due to continuation here: https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1314564/drv8353rs-evm-drv8353rs-evm-motorware-connection-error
Best Regards,
-Joshua
Part Number: DRV8353R Other Parts Discussed in Thread: LM5008 , LM5008A
When VIN =12V(BUCK's bias power) and VM = VDRAIN = 0V, is the internal DC/DC (LM5008) able to be disable by RT/ST pin? and at the same time the gate drivers are shutdown, correct?…