Part Number: DRV8412
Hi,
I am creating the 3-phase stepper motor driver demo via MSPM0 + DRV8412.
I have below 2 questions:
1.
Since the max voltage for motor can not be exceed 6V with Imax 5.5A, may I know if below working conditions are acceptable…
Part Number: DRV8412 Hi team,
why revision H delete values 39-200 in table 6-2? cusotmer used 200kohm as OC adjust resistor, is it not recommended to use this value? if customer continue to use it, what will happen?
Thanks!
Rayna
Part Number: DRV8412 Tool/software: Dear
MP: When using the 8412 parallel drive output and increasing the drive current solution, the peak-to-peak output current of the chip is 7A. The IC is prone to protection. What is the reason for this?
The current…
Part Number: DRV8412
Tool/software:
Hello,
Can i know the reason of this change ? : Changes from Revision G (July 2014) to Revision H (July 2024): Deleted values in 39 to 200 in Table 6-2 .
It's about the Programming-Resistor Values and OC Threshold…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 , DRV8262 Tool/software: Hello,
I would like to ask if it makes sense to replace ( one DRV8432DKD + mounted heatsink) with ( two in parallel DRV8142DKD heat dissipation over power pad)…
Part Number: DRV8412 Tool/software: Hello, I'm using the DRV8412 in parallel mode to drive a thermoelectric unit. It's mostly working but has some issues. It needs to power a TEC module at 5A. I'm testing with a 24V power supply and electronic load. It…
Part Number: DRV8412 Hi,
I have a question about "No external snubber or schottky diode is required" info inside the datasheet. According to datasheet, there is no need for an external schottky diode to protect against back emf fom DC motor. However…
Part Number: DRV8412 Tool/software: As we all know , t he heat dissipation area of the DRV8412 chip is at the bottom of the chip, but in practical applications, if i want to strengthen the heat dissipation of the area where the chip is located, should…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 Tool/software: hi,
As shown in the figure below, DRV8412 is used as an LED lighting driver. Is DRV8412 equivalent to a BUCK circuit? How does DRV8412 work as an LED lighting driver?
Thanks…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8962 , Tool/software: Hi,
1. DRV8432 uses Parallel full bridge with cycle by cycle current limit mode. Occasional triggering of overcurrent protection. Which position is detected for overcurrent…