Hi Loay,
Adding to Pedro's reply, the DRV8434E may also be a good option. It has four half-bridges which can be controlled independently. This device has integrated current sensing and regulation. The DRV8434E is hardware controlled so no serial interface…
Kawasaki-san,
This is the list I have from marketing team. Don't worry about priority column and "N/A" means we don't have a good cross at this time. If you have any specific parts you are missing that are not in this table, please repost…
Hi,
Sorry for the unclear description. And please check if the following updates can help to understand the issue:
Question: How to control a bipolar stepper motor’s rotating direction and speed with DRV8434PPWPR’s AIN1/AIN2+ BIN1/BIN2 control pins?…
Wenting,
The latest PH-EN devices are DRV84xx family. Would you check DRV8424R or DRV8434E to see if it can meeting your requirement? BTW, the DRV8424E/34E full scale current is 2.5A.
Part Number: DRV8812 Other Parts Discussed in Thread: DRV8814 Hi Team,
Due to the lead time issue, the customer is planning using DRV8812 to replace DRV8814.
When the customer using DRV8814, the control of our Drcay pin is Low, so when the motor Enable…