Part Number: DRV8436 Hello, TI.
Should the chip (DRV8436) outputs (A0,A1,B0,B1) be protected using TVS diodes from the pulse noises of nanoseconds and microseconds duration.
Best regards,
Vladimir, development engineer.
Part Number: DRV8436 Customer testing DRV8436EVM with GUI, when customer setting Target speed at 5000, the motor will run a while ,then the motor will stop running. Would you please kindly help to check where is wrong with the setting. thanks !
Part Number: DRV8436E
I'm a little confused on the DRV8436P data sheet.
Assume for the moment we have the xDECAY input driven low (smart tune enabled).
I'm assuming for DRV8436E that, at all times, smart tune chooses the optimal decay mode based…
Part Number: DRV8436 The DRV8436 is on Preview on ti.com, but neither the datasheet nor the product folder shows the mechanical drawing (ie dimensions) of the PWP 24 package. Where can I find it?
Thanks Josef
Part Number: DRV8436 Hi all Would you mind if we ask DRV8436? There is the specification of AOUT and BOUT current matching on the datasheet. We have some questions about it. <Question1> Is it accuracy between Aout current and Bout current? So, if this…
Hello,
As you are always regulating current with a stepper motor, there is not as much margin needed. However, you would be operating near the abs. max and above the recommended max for the DRV8845.
I would consider a device like the following with a…
Hello,
Does it need to be automotive qualified?
If not, please see DRV8426/36.
https://www.ti.com/product/DRV8426
https://www.ti.com/product/DRV8436
Regards,
Ryan
Hi Zhiyuan,
Another alternative part with similar current and voltage rating is the DRV8436. However, this driver is not automotive rated (-Q1).
Regards,
Pablo Armet
Part Number: DRV8434EEVM Other Parts Discussed in Thread: DRV8436 , DRV8434 , Good morning,
I downloaded the firmware package for the DRV8434EEVM and there is no .launch file for it. The launch folder contains the launchfiles for the DRV8436 a but not the…
Part Number: DRV8899-Q1 Other Parts Discussed in Thread: DRV8436 , , DRV8434S Dear team
1. The customer would like to know, is the main difference between DRV8899-Q1 and DRV8436 SPI interface ?
2. Does DRV8899 need to use SPI for initial?
3. Does DRV8436…