Part Number: DRV8436EVM Other Parts Discussed in Thread: DRV8436 Hi Team,
I am trying to confirm the EVM operation of DRV8436.
I installed it with DRV8436-0.0.3.setup-win_7.2.0, What should I use the GUI? I can not proceed to the following screen…
Horst,
The open load detection function has been removed for the new DRV8436. So, I would think you may have an old version device.
Would you share the IC trace code or IC top marking to see if it is an old version device? If it is an EVM, did you…
Josef,
Please check http://www.ti.com/lit/ml/pptd111r/pptd111r.pdf for PWP 24 package or check DRV8436EVM design file to get the layout foot print with the Altium tool.
When DRV8436 is finally released, the datasheet will include the detail mechanical…
Part Number: DRV8436 Customer testing DRV8436EVM with GUI, when customer setting Target speed at 5000, the motor will run a while ,then the motor will stop running. Would you please kindly help to check where is wrong with the setting. thanks !
Ishiwata,
Since the DRV8436 24 pin PWP package will be changed to 28 pin PWP package (extra pin for each output), the DRV8436EVM folder (order link, GUI, user's guide ) is hidden.
The 24pin PWP EVM can still support customers who want to continue…
Betty,
Since DRV8436 PWP package will be changed from 24 pin to 28 pin (4 extra pin for each OUTx pin), the EVM link is hided.
Do you still want the 24 pin PWP DRV8436EVM to do your evaluation? If you can use the 24 pin PWP package DRV8436EVM to do…
Part Number: DRV8889-Q1EVM Other Parts Discussed in Thread: DRV8436EVM , MSP-FET Hi all Would you mind if we ask DRV8889-Q1EVM? We purchased DRV8889-Q1EVM. So, this EVM is the brand new. We tried to operate it, however GUI shows "EVM disconnected" with…