Part Number: DRV8601 Hello,
I'm looking through TI's motor drive/haptic driver portfolios for a device to replace a MAX1749 vibrator motor driver.
I found the DRV8601 to be a decent replacement but was wondering if there are any other similar TI…
Part Number: DRV8601 Other Parts Discussed in Thread: DRV2605 , , DRV2625 Hi team,
A customer is looking for a haptic driver with lowest possible energy consumption. In their application the driver will be off almost all the time, so standby/shutdown consumption…
Part Number: DRV8601 Other Parts Discussed in Thread: DRV2603 I found a list of haptic drivers available from TI at www.ti.com/.../products.html . I will be operating a large number of LRA motors, each of which requires 0.6V AC voltage @ 19 mA, with a…
Part Number: DRV8601 Other Parts Discussed in Thread: DRV2603 Hi Sirs,
Sorry to bother you.
Could you share DRV8601 freq range for us?
Such like DRV2603 spec
Thanks!!
Part Number: DRV8601 Hi,
I am using the DRV8601 to power a 3.3V ERM, at the moment we are powering the motor from a 3.3V 3A bench top supply. So there is no issue with regard to the amount of power but everytime we enable the motor and send a PWM waveform…
Part Number: DRV8601
Dear TI Team,
I am using DRV8601DRBR
As per datasheet, the internal Voltage divider at the REFOUT pin of this device sets the common mode voltage to VDD/2.
But, In our circuit setup as shown below, the voltage at the REFOUT = 0V…
Part Number: DRV8601 Dear TI Team,
I am using an ERM type motor in conjunction with the DRV8601.
The questions are: Enable and PWM of DRV8601 are applied to DRV8601 simultaneously by MCU. (PWM duty 90%) Initially, reverse voltage is generated.
Can the ERM…
Part Number: DRV8601 I ideally would like to GND the themal pad under this IC as I need it to be able to link a GND plane, in the datasheet it states that it has to be connected to the PCB (of course) but it does not state if it can / should also be connected…
Part Number: DRV8601 Other Parts Discussed in Thread: DRV2624 , DRV2625 Hi dear Haptics team,
One of my customers is interested in a haptic driver like the DRV8601.
Are there similar driver with “Error detection”?
Limiting factors are space…
Part Number: DRV8601 Other Parts Discussed in Thread: DRV2624 , DRV2625 , DRV2605 , DRV2605L Hi everyone,
I am developing haptic driver and using LRA .
I couldn't see any information about the frequency of pwm in datasheet. Resonance frequency of the LRA…