Part Number: DRV8601 Other Parts Discussed in Thread: DRV2624 , DRV2625 , DRV2605 , DRV2605L Hi everyone,
I am developing haptic driver and using LRA .
I couldn't see any information about the frequency of pwm in datasheet. Resonance frequency of the LRA…
Part Number: DRV8601 Dear Sir,
We use DRV8601 EVM, connect from PC line out.
We expect Vo=2Vrms when VDD=5.3V,
I modify R1=100Kohms, do you think it will have 2Vrms o/p?
Thanks,Ian.
Part Number: DRV8601
Hi Team,
My customer has a question about the DRV8601 setting.
IN1 input PWM Ferq 3KHz Duty 25% or, 75% or, 25%(5period), or 75%(5period) when EN ON
The vibration amplitude are the same (100%).
How do we to change the input PWM…
Part Number: DRV8601 Other Parts Discussed in Thread: DRV2604 , DRV2605 , DRV2624 , DRV2625 , DRV2603 Hi Team, Do we have solution that can support haptics actuator like DRV8601?
Thanks, SHH
Andre,
Let me give you a call to go over this tomorrow.
I'll use the contact details you provided through e-mail.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Part Number: DRV8210 Other Parts Discussed in Thread: DRV8601 , Hello guys,
One of my customers is considering using DRV8210 to driver Eccentric Rotating Mass (ERM) actuator. And they are considering using DRV8601 too because DRV8601 is a designed device for…
Part Number: DRV8601 Hi, Team
We have a question for DRV8601 reference circuit as below.
Could you let us know what will happen if PWM I/O supply voltage isn't same voltage as VDD?
Does the driver unable to stop the vibrator by change the PWM duty…
Part Number: DRV8601 Reading the datasheet, in section 7.1 it references being able to accept a single-ended DC control voltage to provide a differential output. Can I drive a sensor coil (primary of an LVDT) directly from this device? For input to the…