Part Number: DRV8802-Q1 Other Parts Discussed in Thread: DRV8802 Hello Everyone,
We have developed working prototype using DRV8802 motor driver IC, after developing custom PCB we are facing some issues. We have compared voltage values on all the pins(on…
Part Number: DRV8802-Q1 Other Parts Discussed in Thread: DRV8801A-Q1 , Hi Team,
Can you please help me understand why there is a 1M Ohm resistor between VMx and VCP for the DRV8802-Q1? Also, how come for the same family of devices, such as the DRV8801A…
Part Number: DRV8802-Q1 Hi team,
VM UVLO rising is 7.8V,typ & 8.2V,max, but what about falling?? Is there a VM UVLO hysteresis or de-glitch in DRV8802-Q1?
Thanks.
Dear, Sir.
My customer is looking for Full-step Stepping motor driver.
The driving current is so small as 67mA.
Regarding DRV8802-Q1 ,
Is it no problem to set ISENA/B chopping current as 67mA?
Best Regards,
H. Sakai
Other Parts Discussed in Thread: DRV8802-Q1 Dear all,
I found the difference to recovery OCP between 7.3.7 Table and 7.3.7.1 OCP description at data sheet.
7.3.7 Table says that the way to recovery is ''Retry time, T(OCP)''.
On the other…
Other Parts Discussed in Thread: DRV8881 , DRV8802-Q1 Dear all,
How long does this device take to output transition from xENBL logic high?
Best regards,
Other Parts Discussed in Thread: DRV8802-Q1 , DRV8802 Dear all,
We cannot activate DRV8802-Q1(condition is following and attachment file).
Is there specific sequence to activate this device?
Could you teach me the solutions and the reason why no output…
Other Parts Discussed in Thread: DRV8802-Q1 Hello, Are there the road map of motor driver which have the following specifications?
# of Full Bridges : over 2 Automotiver qualified Operating Voltage range : 6V to 16V Absolute maximum rating : over 32V RMS output…
Dear all,
My customer want to confirm OCP. Is this possible?
Now, they think that R(ISENx) set to 0Ω to seem chopping current setting be invalid.
Is this allowed?
If this is OK, will this device be shutdown within 400ns after over I(OCP)?
*I consulted…
Dear all,
Could you teach me about title at data sheet p.6?
You say that tr = 100~360ns and tf = 80~250ns.
Where these time beins and ends?
Best regards,