Part Number: DRV8806 Other Parts Discussed in Thread: DRV777 Hello;
Is it possible to draw more current by using two DRV8806 in parallel connection ?
If it's not possible, we think that we can use DRV8806 as a gate driver for external MOSFET's. Thus,…
Part Number: DRV8806 Other Parts Discussed in Thread: LM2675 , DRV8860 , DRV8886 Hi Team,
Now, DRV8806 is used as the control solenoid valve. We can control OUT to output VM and GND to achieve control. OUT can normally control the value of OUT with no load…
Part Number: DRV8806 Hİ,
DRV8806 datasheet dedicates that 2-A (Single Channel On)/1-A (All Channels On) Maximum (with adequate PCB heatsinking at 25°C) . Drive Current per Channel (at 25°C).
Additionally I need to know changing of the output current…
Part Number: DRV8806 Other Parts Discussed in Thread: TPS92518 , TPS54286 , , TPS54283 , TINA-TI I need a SPI-controlled buck-regulator with an output ranging from 12V to 24V with 0.5V step resolution. The input voltage is 28V and the max load is 1.5A. I…
Part Number: DRV8806 Hi
I need a high temperature range a driver like the DRV8806 with some clamping voltage pins or simply same function but in operating range (TA) 175°C
Regards
Part Number: DRV8805 Other Parts Discussed in Thread: DRV8806 , DRV8804 , DRV8846 , DRV8884 , DRV8803 , TPL7407L Please kindly help to confirm: Does drv8805 or drv8806 match customer motor to replace sla7033.And please help to recommend more cost-effective…
Hi Bogey,
Please have customer look into the DRV8823-Q1 and DRV8824-Q1 stepper motor driver. Let us know if there are specific question about the devices. Thank you.
Other Parts Discussed in Thread: DRV8805 , DRV8806 , DRV8805EVM , DRV8880 Hi,
It does not determine to what the control signal, it uses 2A of UNIPOLAR STEPPER MOTOR.
(Continuous current is scheduled for approximately 1.4A)
DRV8805 and DRV8806 or is suitable…
Other Parts Discussed in Thread: DRV8806 Hi, I have configured three DRV8806 in daisy chain connected to a SPI module of my MCU. The clock , the latch and data IN seems to act correctly. Enable signal is active and reset signal is inactive. For a unknown…
Part Number: DRV8803 Other Parts Discussed in Thread: DRV8806 , DRV8860 , Dear TI,
Disconnection issue occurred while reviewing Motor Driver.
We are currently testing with Zener + UFD as follows.
1. Disconnection issue Waveform
2. Zener + UFD be used
…