Part Number: DRV8818 Other Parts Discussed in Thread: DRV8424 I am testing the TI DRV8818PWP as a replacement for an Allegro A5977. An observation has been made that the first step after crossing zero A has a current oscillation that it not present with…
Hi Pablo, besides RCA and RCB we also tuned the current holding current to get rid of the noise. Jan already explained this action. We did not succeed to take it away completely. We still have 10 to 15% that produce noise and therefor do not pass the test…
Part Number: DRV8818 Other Parts Discussed in Thread: DRV8424 Dear TI-er.
I saw the link below.
https://www.ti.com/lit/an/sloa312/sloa312.pdf
Can I use DRV8818 to ignore the center tap on each winding for unipolar motor ?
My customer want replace SLA7078MS…
Part Number: DRV8818EVM Other Parts Discussed in Thread: DRV8811EVM , DRV8811 , , DRV8818 Hi team,
My customer needs DRV8811EVM for evaluation, but cannot find any stock from TI or disty.
Can we use DRV8818EVM? It seems possible if we replace DRV8818 chip…
Part Number: DRV8818 Hi,
In the datasheet, on page17, 8.2.2.2, IFS = VREF/(A*Risense) and in example, To achieve IFS = 1.25 A with RSENSE of 0.1 Ω, VREF should be 1.56 V.
Is this equation correct?
With 1.5V Vref, 0.2Ohm Risense, circuit is limited by…
Part Number: DRV8818 Hi team,
How do I set the pin to keep the motor functional? i.e. when moving to a specified position, the motor does not move and is applied torque.
Could you help resolve this case? Thanks.
Best Regards,
Cherry
Part Number: DRV8818 Other Parts Discussed in Thread: DRV8434S , DRV8434A Hi team,
The customer intends to use use the DRV8818 to drive the stepper motor, and now would like to know the maximum continuous output current of the device, and is this continuous…
Part Number: DRV8818 Hi Team,
We would like to ask your your help regarding our customer's inquiry below.
We have use the stepper motor driver chip to drive a unipolar stepper motor with following specification,
Part number: PJB42S33D16
Step Angle…
Part Number: DRV8818 Other Parts Discussed in Thread: DRV8424 Dear Forum, Dear TI Experts,
we replaced a stepper motor driver due to EOL notice. On the legacy board, it was used a stepper motor driver from Allegro Micro Systems. A3977SED-T ( Stepper Motor…