Other Parts Discussed in Thread: DRV8832 , DRV8832EVM I'm designing an MCU interface between a PIC18F67J11 (3.3v) and a DRV8832. My motor is a 6V DC brushed motor. I want to use the iSense capability to limit current to 400 or 500mA. I do not need variable…
Hi Dev,
Dev_Ninja said: 1- Motor current at OUT1/2 is limited to 1A internally, however in the first page of the datasheet shows 1.3A peak to the motor, see picture below. What's the true maximum current that can be supplied to the motor?
1-A peak…
Other Parts Discussed in Thread: DRV8832EVM , DRV8832 Hello,
Please send me Orcad symbol of the chip and schematics in Orcad format for DRV8832EVM.
Thanks.
Igor
Hi again.
I have now purchased an DRV8832EVM evaluation board to which I have feeded the same IN1 and IN2 signals as on my proprietary board. And I can see on the oscilloscope that an identical FAULTn pulse appears on the demo board. So now I start…
Other Parts Discussed in Thread: DRV8832 , L293D , TMS320F28027 , DRV8832EVM , DRV8837 Hi guys,
I'm going to fabricate my first PIC-like F28027 main board, where I'm going to drive a small motor using TI's DRV8832 .
BUT before that, just a quick question…