Part Number: DRV8837C Hi Sirs, Is there side effect if we violate the fall time specification (for example, when the fall time faster than 20ns or slower than 188ns)? Should we add a small cap at output pins if the fall time is faster than 20ns? Thank…
Part Number: DRV8837C Other Parts Discussed in Thread: DRV8837 Hi Sirs, My customer would study the DRV8837 to drive an IR Cut Module based on the application note of http://www.ti.com.cn/cn/lit/ug/tidue56/tidue56.pdf Would you please advise if product…
Part Number: DRV8837C
Hello
I have seen the datasheet for motor driver drv8837c . Following are the queries:-
1>Whether it is Half H bridge or Dual H Bridge?
2>In the Evaluation Board of drv8837c , the jumper connections are used to change the…
Part Number: DRV8837C Other Parts Discussed in Thread: DRV8837 Hello,
DRV8837 has C and no C, What does it mean to have a C?
I confirmed the difference in the attachment.
Best regards, DDdoor
Part Number: DRV8837C Other Parts Discussed in Thread: DRV8212 , DRV8837 Dear Teams,
My customer is using DRV8837C for their smart lock end equipment. They have following questions would like to confirm:
The Iocp (min) is 1.2A, and the tDEG is 1us…
Part Number: DRV8837C Hi there,
I am interested to find out if the component can be used in Class 2 medical devices.
Also if it is possible, the operating relative humidity (RH) and operating pressure.
Thank you!
Jim,
250kHz cycle time is 4us.
1us Overcurrent deglitch time; 160us maximum INx to OUTx delay; 188ns maximum output rising and falling time; input noise deglitch filter are all in this 4us. Also, the charge pump circuit need to support the integrated…
Part Number: DRV8837C Dear Sirs,
My customer asked us about The behavior on the forced operation of DRV8837C.
In case the DRV 8837C is automatically operated in one direction and forcibly stopped from the outside and moved manually in the opposite…