Hi Kevin,
The DRV8837EVM can be modified to allow external control. Please refer to the schematic. R3, R4, and R5 can be removed.
If you prefer to use a wson to dip board, I suggest you search online for a conversion board.
Other Parts Discussed in Thread: DRV8837 , DRV8837EVM I'm using DRV8837 to drive a RC toy motor. There are two motors, very similar, from the same Chinese supplier, recommended at 3.7V. The only difference is the size:
- the right one is 7mm diameter…
Fatin,
Rise/fall times for DRV8837 are typically 100ns with a max. of 150ns as given in the datasheet. Although, I have to be honest and am not sure what the load was under these test conditions and for your load it will surely be different.
The EVMs…
Other Parts Discussed in Thread: DRV8801 , TPA2005D1 , DRV8837EVM Hi everyone,
I am looking for a chip to convert an analog signal into a pwm signal to control the DRV8801. The pwm signal output should be about 32kHz. I found this chip : http://www.linear…