Part Number: DRV8860 Hi,
We use the DRV8860 for our IO module low side driver, and now, we find there are some quiescent current when the output closed, the current is about 20uA, the LED on the backend will light up so please advise how to eliminate…
Part Number: DRV8860 Tool/software: Hi,
We use the DRV8860 for the low side IO module control, and now, After reading and clearing the fault, there will be two open leakage faults that do not output and sometimes have data errors.
The attachment is…
Part Number: DRV8860 Hi TI E2E Support Team,
We recently received a new batch of DRV8860PWPR ICs, but the top-side markings and internal structures differ noticeably from our previous, known-good batch. Our assembly house assures us that the new batch…
Part Number: DRV8860 Tool/software: Hi
Please recommended a LDO or DC-DC Converter power supply for DRV8860 and 6 solenoids total current will be around 1.12A. as per our application the Input voltage to regulator will be 11.6V-12.6V Nominal 12V and…
Part Number: DRV8860 Tool/software: DRV8860 Driver recommended VM Motor power supply voltage range is 8V to 30V. Our requirement is to drive 6 solenoids on of voltage rating 9V and each solenoid current rating is 188mA .
Can we connect the VM pin to…
Part Number: DRV8860 Tool/software:
Hello.
I'm working on a revamping project that has to drive six electrovalve ( 24V 150ma each). In order to reduce the total power absortion i'd like to switch on a PWM 50% after some 10ms As far i've understand…
Part Number: DRV8860 Tool/software: Hi expert,
Could DRV8860 DOUT pin left floated? We are trying to use 2 chips DRV8860 (U1 DOUT connect to U2 DIN) but no need for fault reading so left U2 DOUT floated. Is there any problems?
And we found when powered…
Part Number: DRV8860 Tool/software: Hello,
DRV8860PWP drives stepper motor. During the testing process, it was found that the waveform of the output pin was abnormal, as shown in the following figure. Please help analyze the cause.
The schematic…
Part Number: DRV8860 Tool/software: Hi TIer
My customer use DRV8860 to drive the Valve .
We parallel 4 output in one chip and to drive this valve.
because valve only 3ohm and 24V/12V support so we need choose PWM method to control the valve. …
Part Number: DRV8860 Other Parts Discussed in Thread: DRV8803 , DRV8932 Hello
I was looking at the DRV8860 for a solenoid control application - I hit the solenoid with 100% duty cycle and then hold a 50% duty cycle. But, I need the solution I choose…