Part Number: DRV8871-Q1 Other Parts Discussed in Thread: DRV2605L-Q1 , , DRV2605L Please confirm whether the PWM/output signal from the DRV2605L-Q1 can be connected to the control input of the DRV8871-Q1, allowing the DRV8871-Q1 to switch a 16 V supply…
Part Number: DRV8871-Q1 Hello, I'm very sorry to disturb you. Regarding the material "DRV8871DDARQ1" with a humidity and temperature rating of MSL3, the vacuum bag is not leaking. The production year cycle is 2025, with 29 weeks of production. However…
Part Number: DRV8871-Q1 Dear team,
My customer wants to use our device to drive a coil, and there will be bidirectional current on this coil. In addition, this coil has a special feature, when the current flowing through the coil is less than 0.1A,…
Part Number: DRV8871-Q1 Other Parts Discussed in Thread: DRV8871 , DRV8872 I have developed a board that is intended to drive different types of motors. One application is a "smart" servo motor which has an integrated controller and an RC (PWM) interface…
Part Number: DRV8871-Q1 Hi,
I am working with this part to drive a motor with this characteristics
No Load Current = 150mA
Stall current 4A max
I set the H-bridge for max current limit of 3.5A so it never reaches lock current, and I am PWM @ 400Hz…
Part Number: DRV8871-Q1 Hi team,
Greetings. I have a question about the VM bulk cap of DRV8871-Q1.
The parameter is that VM=12V coming from automotive battery, normal working current=1A, stall current=2.5A.
Duty cycle is 100% only using high or…
Part Number: DRV8871-Q1 Dear, Sir.
My customer is looking for the alternative part instead of TA8050FG/Toshiba.
I am thinking DRV8871-Q1 would be suitable for that.
As the double-confirmation, I would like to make sure the Rds(on) definition.
…
Part Number: DRV8871-Q1 Hello Guys,
Our customer is driving a toroidal inductance of about 500uH (not a motor). As he understands it, in order to "change direction" there are inductive effects to related to changing the direction of the current need…
Part Number: DRV8871-Q1 Dear, Sir.
My customer is considering to apply DRV8871-Q1 for their system.
They don't have an experience for thermal pad soldering because the inspection
is impossible. So, they are asking about the thermal performace degradation…
Part Number: DRV8871-Q1 Hello,
Our customer is looking for a way to sense the current flowing through the motor. Can they have a sense resistor between Pin 7 (PGND pin) and Power ground?
Regards,
Roland