Part Number: DRV8874-Q1 Hello,
I was verifying the Auto-Retry mode on the OCP feature and I got these scope shots:
CH1: VM, CH2: IOUT, CH3: OUT1 CH4: nFAULT
The setup is using Auto-Retry OCP mode with an E-load trying to draw about 9A from OUT1 and OUT2…
Part Number: DRV8874-Q1 I found out the wire bonding of DRV8874QPWPRQ1 is consisting of Cu.
Can you please confirm whether we had qualified AEC-006? Thank you.
Part Number: DRV8874-Q1 Hi team,
TI's motor drive IC DRV8874-Q1 output overcurrent protection, IPROPI pin configuration resistor sets the maximum overcurrent, how long does Iout fall when the output current reaches Itrip? The customer would like to k…
Part Number: DRV8242-Q1 Other Parts Discussed in Thread: DRV8874-Q1 , DRV8874 Hello Team, customer want to change from DRV8874-Q1 to the recommend new DRV8242-Q1.
Big difference is the specified maximum PWM frequency:
DRV8874 - PWM frequency up to 100…
Part Number: DRV8874-Q1 Hi team,
Issue: The circuit is designed according to the current detection in the manual and calculation is according to the corresponding equation. But the measured result does not correspond to the equation.
The chip is now configured…
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8876-Q1 Hi team,
My customer is asking for peak driving current versus ambient temp curve.
They would like to know the driving current variation when TA temp increased?
But there is no this kind…
Part Number: DRV8874-Q1 Other Parts Discussed in Thread: DRV8714-Q1 , DRV8873-Q1 , DRV8718-Q1 , Hi,
I have a question from a customer.
is there a recommended automotive door lock actuator for this device?
I would be grateful if you could get information that…
Part Number: DRV8874-Q1 Hi team,
We are considering this type for rotary solenoid drive.
If you have an open / short test report for future development, please provide it.
Regards,
Hitoshi Koide
Part Number: DRV8874-Q1 The circuit designed according to the current detection in the manual is also calculated according to the corresponding formula. The current situation is that the measured results do not correspond to those calculated by the formula…
Part Number: DRV8874-Q1 Hi team,
Do you have a pitch conversion board for HTSSOP16?
Or is it possible to get DRV8874-Q1 sample on a pitch conversion board?
Regards, Ochi