Part Number: DRV8899-Q1 Other Parts Discussed in Thread: DRV8873-Q1 , DRV8876-Q1 , , DRV8245-Q1 , DRV8145-Q1 Hi, TI,
I would like to check with you about the leakage on AOUT1, AOUT2, BOUT1 and BOUT2, when driver outputs are disabled (Hi-Z state)? and i want…
Part Number: DRV8876-Q1 Hi team,
Do you have recommended capacitance about "CBulk" in "Figure 19. Typical Application Schematic"?
Or could you tell me how to calculate "CBulk" value?
Regards, Ochi
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8876 Hi Expert,
Could drv8876-q1 regulate the speed of motor? Our device is used to drive an electric fan to cool CPU.
Thanks
BRs,
Wilson
Other Parts Discussed in Thread: DRV8876-Q1 Hi TI,
I am trying to Simulate DRV8876-Q1 PSpice in OrCAD Latest version 2023 but it showing some error can you help me out to resolve.
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8801-Q1 , Hi Expert,
I need a Q1 level(use for auto) motor driver device to drive the DC motor in electronic lock.
I only need a +12V output to open the lock motor, and a -12V output to close the…
Part Number: DRV8876-Q1 Other Parts Discussed in Thread: DRV8873-Q1 Hi, Does DRV8876-Q1 have "Open load detection" function? The customer intends to connect two loads in Independent Half-Bridge Control Mode. If it has that protection, could you…
Part Number: DRV8876 Hello! Datasheet of DRV8876 is unvailable as of this writing. Can we use DRV8876-Q1's datasheet temporarily? Are there major differences between the two? Thank you!
Part Number: DRV8876-Q1 Hello
My customer is interested in DRV8876-Q1.
I see DRV8876-Q1 is same except AEC-Q100 qualified , but is it correct?
When RTM is available?
Best Regards
Part Number: DRV8876-Q1 Hello
We found that the motor driver provides a current in both directions( limit of -7.5mA to +7.5mA ) depending on the rotation direction of the motor.
So does that mean the output on the pin "IPROPI" will be a negative value when…