Part Number: DRV8904-Q1 All bit fields of "OP_CTRL_2" , "OP_CTRL_3" and "FW_CTRL_2" are Reserved.
What action does the driver take when sending an instruction to write data of "0x00" to "OP_CTRL_3" and "FW_CTRL_2" ?…
Part Number: DRV8904-Q1 Other Parts Discussed in Thread: DRV8874-Q1 , DRV8876-Q1 , DRV8876 Hello,
My customer is interested in DRV8904-Q1, but they'd like to have >2kHz from the PWM generator. If I understand correctly, DRV89xx-Q1 devices can output…
Part Number: DRV8904-Q1 Hi team,
1. For DRV8904, it ’ s dual H bridge, and each channel peak driver current to 1A, from the application schematic, seems can realize parallel connection to increase the drive current range. If do this application, has…
Okay good, then it is likely not TSD.
Let me know what you find, I am interested!
If this is a new design, would you be interested in a newer part? DRV8908-Q1 might be a better fit for you at a lower price and double the channels (or DRV8904-Q1 for 4-channel…
Hi Kazuya,
1. VDAC is the Digital to Analog Voltage.
2. Yes, that is the average range that can set VITRIP through SPI.
The DRV8243-Q1 can be used for latching solenoids and is typically not used in a peak and hold application.
The DRV89xx-Q1 family of…
Part Number: DRV8889-Q1 Other Parts Discussed in Thread: DRV8904-Q1 1.Can I drive Unipolar Stepper Motorswith DRV8889?
2If possible, are there any relevant literature references?
Part Number: DRV8908-Q1 Hi team,
Our customer want to use one piece DRV89XX family(8904/8908/8912) to drive different types of motors: stepper motor, brushed DC motor and delay simultaneously.
Just using one DRV89XX's different output channels for different…
Part Number: DRV8904-Q1 I want to use DRV8904-Q1 as a low side switch in an automotive solenoid driver.
Options:
1) Use the body diode of the high side FET
2) Use an external diode for the free wheeling current
3) Use the high side FET to carry the free…
Part Number: DRV8904-Q1 TI,
I am looking to use the DRV8904-Q1 to operate 4 independent small motors uni-directional. I am assuming that I can use each channel of the DRV8904 to operate an individual motor via internal independent 8-bit PWM. I would connect…