Hey Stefan,
Admittedly we don't appear to have anything perfect for this application.
One option is DRV8847 - it has independent 1/2 bridge control and current regulation, so you could use it to drive 4 of the 6 solenoids.
Another is DRV8906-Q1 , though…
Other Parts Discussed in Thread: DRV8910-Q1 , DRV8904-Q1 , DRV8906-Q1 , DRV8908-Q1 , DRV8912-Q1 DRV89xx-Q1 (DRV8904-Q1,DRV8906-Q1,DRV8908-Q1, DRV8910-Q1, DRV8912-Q1) device has internal PWM generator. When PWM Duty is set as FFh(max), it is very close to 100…
Part Number: DRV8908-Q1 Other Parts Discussed in Thread: DRV8904-Q1 , DRV8906-Q1 , , DRV8912-Q1 Hi team,
One of my customer wants to use the same PCB with different DRV89XX to adapt different products. Can DRV8904-Q1 / DRV8906-Q1/DRV8908-Q1/DRV8912-Q1 be …
Part Number: DRV8910-Q1 Hello!
What are the differences between the DRV8910 and DRV8908 except for the number of channels?
Not only DRV8908 have less bonding wire, are the chips different?
What are the differences between the DRV8908 and DRV8906 except…
Leslie,
Thank you!
Marc,
Specifically, please see the DRV8906/8/10/12-Q1 (SPI controlled integrated 1/2 bridge family) devices and the DRV8243/4/5-Q1 (high power integrated driver family) devices. Those should cross with all of the above.
Regards,
Ry…
Part Number: TPS2H160-Q1 Hello Team,
customer needs for worst case calculation a chart about thermal impedance (Zth) over time. Similiar what we did in our motor driver datasheet i.e. DRV89xx chapter 9.3.4 - transient thermal.
DRV8906-Q1 data sheet, product…
Hi Ochi san
To support 3A motor + others(LEDs), DRV8912-Q1 is better than DRV8906-Q1 for thermal view point. If you drive 3A contious with 3 H bridge, die temp may be too high under high Ta(e.g)85C.
Then Customer can use 4-5 H bridge for 3A with parallel…
Hi,
DRV8908-Q1 has 8ch half bridge and each channel can drive 1Arms. With parallels mode of 2ch combined, can drive 2Arms. Therefore 2pcs of DRV8908 can support 2A(by 2ch) x 8 low side drivers.
Other families are DRV8912(12ch), DRV8910(10ch).DRV8906(6ch…