Part Number: DRV8910-Q1 Hello!
What are the differences between the DRV8910 and DRV8908 except for the number of channels?
Not only DRV8908 have less bonding wire, are the chips different?
What are the differences between the DRV8908 and DRV8906…
Part Number: DRV8910-Q1 Hello !
Customers requests critical circuits to be aging tested before shipment.
Are the following parts aging tested before shipment?
DRV8910
DRV8244
Please tell me about the contents of inspections that can be disclosed…
Part Number: DRV8910-Q1 Hi Team,
I'm trying to understand why a false flag can occur during current re-circulation if synchronous rectification is ON?
Also why IOUT2_LS below IOLD will trigger a fault? Does it mean that detecting circuit is still…
Part Number: DRV8910-Q1 Hi,
my customer is using DRV8908, but wants to regulate 8 half bridges with PWM.
Can he continue using DRV8908, or how many PWM outputs are integrated?
If DRV8908 does not work, would 2xDRV8904 an alternative?
Kind…
Part Number: DRV8908-Q1 Other Parts Discussed in Thread: DRV8912-Q1 , DRV8910-Q1 Tool/software: Hi team,
Customer is considering the risk of mix populate different DRV89XX version, would you pls help us understand using below two scenario as example;…
Other Parts Discussed in Thread: DRV8910-Q1 , DRV8904-Q1 , DRV8906-Q1 , DRV8908-Q1 , DRV8912-Q1 DRV89xx-Q1 (DRV8904-Q1,DRV8906-Q1,DRV8908-Q1, DRV8910-Q1, DRV8912-Q1) device has internal PWM generator. When PWM Duty is set as FFh(max), it is very close…
Hi Sonal,
Thank you for posting on this forum. You mentioned NCV7720 in the title of this post. The on resistance of this device is specified at 1 ohms in its datasheet. This is a 10x half-bridge driver with SPI interface. An equivalent option from…
Naveen,
SCLK minimum high or low time is 100ns. Some pulses just give about 100ns high or low time. Is it a real scope waveform or a simulation waveform? The edge looks so sharp. Would you slow down the clock?
0x4700H was sent to the SDI, you get…