Part Number: LMK1D2102 Other Parts Discussed in Thread: DS25BR150 , Hi,
I have a number of very low jitter clocks coming offboard. I am looking for a buffer to restore the clocks in the 100MHz - 1GHz range with the lowest possible jitter.
Is LMK1D2102 suitable…
Other Parts Discussed in Thread: DS25BR150 , DS38EP100 , DS25BR101 , DS25CP104A Dear Team,
do you have a redriver, retimer, buffer or a similar IC for Sony Low voltage LVDS ( subLVDS)?
Vcm=0.9V
Vod = 150mV
Best Regards,
d.
Part Number: DS25BR150 Other Parts Discussed in Thread: DS25BR110 Hi HSI team,
I have the following questions:
Can FPD-III be range extended
How to work with the back channel?
Seems, it cannot be disabled by software
Is it in lower frequency range…
Part Number: DS25BR150 Hello,
I would like to verify electrical compatibility between Transceivers TX Cyclone V and DS25BR150 : TX cyclone V electrical level : PCML, my configuration=AC coupling
CY V TX PCML AC coupling -> LVDS DS25BR150
Could you…
Part Number: DS25BR150 For the DS25BR150:
What happens when both inputs are tied to ground?
What about when one is tied to ground and the other is floating?
What about if neither inputs are used, how should they be tied?
Part Number: DS25BR100 Other Parts Discussed in Thread: DS25BR120 , , DS25BR110 , DS25BR150 Hi team,
My customer wants to know the Air Gap Discharge Protection spec of below device. The customer wants ±8kV as the spec. If you have the spec, please let…
Part Number: DS25BR150 Other Parts Discussed in Thread: DS25BR120 , DS25BR100 , , DS25BR110 , DS90LV004 , DS15MB200 , DS25BR440 Dears,
I am looking for a LVDS buffer that support Hot Swap. But can not find a direct solution. Can you please comment and suggest…
Part Number: DS25BR150 Hi do i need some external pull up/down resistors if i have no driving output connected to the ds25br150 input?
thanks for your answers
br
Other Parts Discussed in Thread: DS25BR150 Dear Sir/Madam,
There are queries which need inputs from the company for the following part: DS25BR150
1) What is the process technology used to fabricate the DS25BR150 , is it purely based on bipolar technology…
Hi Malik, Thank you for your reply.
I'm looking for a buffer to convert the SLVDS output of the ADC36632 (2CH) to LVDS, as in the attached signal chain. I consider DS25BR150(1CH x2), however, if you have any recommended device, let me know.
<Other request…