Part Number: DS30BA101 Other Parts Discussed in Thread: DS30EA101 Hello, I would like to use the DS30BA101 and DS30EA101 to transmit and receive 8b/10b encoded data over 50 ohm coaxial cable. The cable is about 1 meters long and data rate is 3.125Gbps…
Part Number: DS30BA101 Other Parts Discussed in Thread: DS30EA101 , LMH0302 , LMH0303 Hello, I would like to use the DS30BA101 and DS30EA101 to transmit and receive 8b/10b encoded data over balanced 150 ohm cable differentially. The cable is about 4 meters…
Hi Mark,
The max insertion loss can be estimated by knowing two parameters:
1. EQ Gain Capability of the DS30EA101: From Nasser's previous post , the EQ capability is 16 dB at the Nyquist frequency of 200 MHz, assuming the source is outputting 800…
Part Number: DS30EA101 I am using the DS30EA101 and I wanted to know if it matters how close I put my capacitors, resistors, and inductors in relation to the BNC connector. Do these components need to be close to the BNC connector? Does it matter where…
Hi Mark,
I was unable to view the images you attached, but I think I am able to get the gist of what you are requesting.
In the figure, we typically place the AC coupling capacitors after the terminating resistor so that the impedance discontinuity…
Part Number: DS30BA101 Other Parts Discussed in Thread: DS15EA101 , DS30EA101 Hi Team,
Could you please allow me to ask about DS30BA/EA101 cable extender device ?
One question we have is that if this device pair could be used with single end 50 Ohm…
Other Parts Discussed in Thread: DS30BA101 , DS30EA101 Hi,
I have a SDI signal from a serializer on an electronic board, and a deserializer on an other electronic board.
I plane to use DS30BA101 and DS30EA101, with a twisted pair cable as explane…
Part Number: DS30EA101 Other Parts Discussed in Thread: LMH0394 Is there a pin and footprint compatible part to the DS30EA101 that is just a buffer and does not have equalization capabilities (or can be turned off)?
I am using this part in the system…
Other Parts Discussed in Thread: DS30BA101 , DS30EA101 Hello,
In regards to LVDS buffer/equalizers, P/N: DS30EA101 and DS30BA101, the input spec for the ‘EA101 says 720mVp-p min at 0m cable length. What is minimum with say 5m cable or 10m cable? I’m…