Other Parts Discussed in Thread: DS64MB201 Hi, We are planning to use the chip 'DS64MB201' for QSGMII signal switching between devices.
we are trying to simulate TI Mux Tx to Device Rx path (in hyperlynx). In simulation, Signal amplitude goes above…
Other Parts Discussed in Thread: DS64MB201 Hi Team,
Our customer is observing the following symptom. They have same signal input to SIA0 and SIB0. When selecting the input using SEL0/1 pin, DOUT0 waveform shape of DE changes in random. We guessed the Auto…
Hi,
The driver de-emphasis DEM is an RC filter to improve the eye after the channel loss.
The bit 7 is to enhance / improve the signal at the higher data rate by reducing the DEM pulse width.This helps to improve the eye for the high data rate signal (6Gbps…
Other Parts Discussed in Thread: DS64MB201 hi, I write DS64 register 0x2 to 0x1 when power up, and the default value is 0x0, after the SersDes signal pass through the buffer, sometimes this register change to 0xff, and single can't pass it, I don't know…
Other Parts Discussed in Thread: DS100MB203 , DS64BR401 , DS64MB201 Hi, could you please let me confirm about the Junction Temperature description in the datasheet ?
In the datasheet P.5 Junction Temperature Range is said as "+105C" for TJ(MAX…
Other Parts Discussed in Thread: TPS54426 , DS64MB201 , DS64BR401 Our customer is considering to power the device with DC/DC converter, TPS54426.
What is the recommended power design for DS64MB201 ?
If you see the User Guide of DS64BR401, I found EVB is…
Other Parts Discussed in Thread: DS64MB201 , DS100MB203 Please let me ask the LVCMOS input specification for DS64MB201.
[Question]
Are all the LVCMOS input pins 3.3V tolerant ?
I am understanding that SDA/SCL is 3.3V tolerant, but if you read the Absolute…
Other Parts Discussed in Thread: DS64MB201 Hi, please tell me what to do with the unused input/output channel pins of DS64MB201.
1) SIA and SIB, DIN0 and DIN1 input pins
--> As the input have signal detect circuitry, leaving OPEN seems to be the best…
Hi Hossam,
Perhaps DS64MB201 may meet your requirement. Please below note a link to this part's data sheet:
https://www.ti.com/lit/ds/symlink/ds64mb201.pdf?ts=1635550933975&ref_url=https%253A%252F%252Fwww.ti.com%252Fsitesearch%252Fdocs%252Funiversalsearch…