Part Number: DS80EP100 Hi expert,
I am found a suitable deive for SLVS-200(Scalable Low Voltage Signaling - 200 mV) cable compensation, the SLVS-200 signal parameters are as below:
For the system, the IC need to cover the cable loss from type-C…
Part Number: DS80EP100 Other Parts Discussed in Thread: DS38EP100 , EQ50F100 Hi,
I have customers who want to use this chip to drive and balance CML, because their Serdes running speed may be lower than 5G, this chip IN OUT mode, if it is lower than…
Other Parts Discussed in Thread: DS80EP100 , DS38EP100 , DS90LV001 Hi TI,
I am looking for an LVDS equalizer product.
1. Using Main frequency 288MHz. 2. Use only Receive Equalization during Pre-Emphasis and Receive Equalization.
DS38EP100 or DS80EP100…
Hi Kawai,
Yes the DS80EP100 can be used with OOB signaling. Since this equalizer design is passive, the overall voltage gain at the OOB frequency will be about -6 dB or about 50% of the input level. This should still be enough voltage to have good OOB…
Hi Kawai-san, I just received feedback from our Product Engineer: The marking of on the IC is done in the following format for the DS38EP100:
YM = YEAR MONTH DATE CODE L = LAST DIGIT IN ASSY LOT CODE The marking of on the IC is done in the following…
Part Number: DS30BA101 Other Parts Discussed in Thread: DS80EP100 Tool/software: Dear Team,
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/538679/redriver-for-fpd-link-iii-we-are-using-ds90ub948-ds90ub947
i refer above thread…
Part Number: TLV3801 Other Parts Discussed in Thread: DS90LV001 , DS38EP100 , DS80EP100 , DS25BR110 , LMK04228 , I have a few LVDS signals coming off-board. Can I use this part to restore the eye diagram and provide very low jitter for the external LVDS…
Part Number: DS38EP100 Other Parts Discussed in Thread: DS80EP100 , Hello Support team,
Is it possible use DS38EP100 and DS80EP100 as bridge LVDS to LVPECL and LVPECL to LVDS?
Best Regards, Hirokazu Takahashi